I bought two Bluetooth DIP modules and i’m triying to make a connection between them. I connected the first module to my PC and the other module to power, and i shorted the RTS and CTS lines and TS and RX lines with no connection.
When i perform a discovery any bluetooth module is displayed, can you tell me what am i doing wrong?

I’m using a bluetooth dip module and have only had it connect to my PC once!
I’ve connected the bluetooth dip module to the FTDI seria/usb module that also powers it. I can interrogate the device, but my PC with a bluetooth usb dongle running bluesoleil simply doesn’t recognise it. I’ve tried two of the same type of dongle as weel as my mobile phone and pocket pc.
Is there something obvious I’m missing?
Hello,
The most of the problems with the DIP module ocurr because under the antenna there are something metalic.
Try to put the DIP module in a protoboard in the bottom of the board so you dont have any metalic lines under the antenna, it should work
if you have any doubt email me, the direction is in my web site http://eguezgustavo.webcindario.com
is in spanish…