Bluetooth in 10.3.9, Plus WiTilt with serial in Max/MSP?

Hey anyone got wiTIlt V2 to work with the serial object in Max?

Also I wonder if there’s something I’m missing in the docs.

Bluetooth set-up in 10.3.9 won’t take “default” as a pairing number.

Works in 10.4.5. Anyone know a work around for OSX 10.3.9?

Also…

I can get WiTilt to work with terminal using the cmd “screen”

in OSX 10.3.9 & 10.4.5 but the config requestor will not quit unless I force quit the screen command.

Is there a general quit / sign off cmd to send the WiTilt unit to

break contact cleanly with no hanging processes?

thanks -Teflon.