Bluetooth Mate Silver question

I’m trying to measure the signal strength of the bluetooth signal from my laptop using the Bluetooth Mate Silver with an RF detector. The RF detector has an input for the received RF signal and it outputs a voltage proportional to the signal strength.

Here’s my question: Is the RX pin on the Bluetooth Mate Silver the point at which the received signal could be measured (that would be input to an RF detector)? I really only want to use the Bluetooth Mate Silver as an antenna to receive the signal from my laptop that is paired with it.