Bluetooth Networking Has anyone had success creating a stand

Anyone have experience in successfully creating a standalone network using bluesmirfs, without using a pc to host?

faultsprofit:
Anyone have experience in successfully creating a standalone network using bluesmirfs, without using a pc to host?

Yes, you can run them ad hoc, but you have to make one device discoverable so it can run as the hub, and it must be paired with your other devices. So far I don’t see a way to make it automatically link up with anything it hasn’t been paired with like a bluetooth hotspot can (if running in insecure mode), but if you pair everything and use the AT commands to make it automatically connect to incoming requests, if paired it should pick up and act like a hub, networking all your devices, paired or not up to the usual bluetooth maximum of 5 connections per device. After that it’s seamless since it’s all a bridge protocol.