Hi all,
We’re having real problems trying to get our Bosch BMV080 working consistently with our raspberry pi for a proof of concept. Below is a summary, any advice or help would be very much appreciated!
Hardware Setup
- Device: Raspberry Pi running Linux 6.12.25+rpt-rpi-2712
- Sensor: Bosch BMV080 particulate matter sensor
- Connection: I2C bus 1, address 0x57
- Sensor Detection: Successfully detected with sudo i2cdetect -y 1
Software Components
- BMV080 SDK: Version 24.1.0.0dd757a809c.0
- Binary location: /home/j501/ScanNeo/AQMonitor/api_examples/raspberry_pi/bin/armv8-a/aarch64-linux-gnugcc/release_i2c/bmv080_example
- Compiled for ARM64 architecture
- Runs with command: ./bmv080_example i2c - Flask API Service: Running on port 8082
- Endpoint: http://192.168.1.154:8082/air-quality
- Attempts to read sensor every 10 seconds
- Returns 503 when sensor fails
Error Codes Encountered
- Error 133: “Opening BMV080 sensor unit failed with BMV080 status 133”
- Most common error
- Occurs during sensor initialization
- Indicates communication or power issue - Error 114: “Opening BMV080 sensor unit failed with BMV080 status 114”
- Occasionally appears instead of 133
- Also an initialization failure - Error Sequence When Partially Working:
- Error 211: Data fetch failure
- Error 403: Data fetch failure
- Error 214: Repeated data fetch failures
- These occur AFTER successful initialization but during continuous reading
Observed Behavior
- Intermittent Operation:
- Sometimes initializes successfully (shows “Sensor ID: D0LP19152509”)
- Provides 3-5 valid readings (PM1, PM2.5, PM10 values)
- Then fails with errors 211, 403, 214 - Current State:
- Consistently failing with error 133
- Cannot initialize sensor
- I2C device still visible but not responding properly