I found a nasty bug in the datasheet.
I was programming the spi port an olimex LPC-1343 board to connect a kent display.
I wanted the spi clock on PIO2_11 (connected to uext.)
no way to get a clock work, after a lot of time spent to track the signal with an oscilloscope,
I finally I discovered that the information in the datasheet was wrong
the datasheet say:
2:0 FUNC Selects pin function. All other values are reserved. 000
0x0 Selects function PIO2_11.
0x2 Selects function SCK0 (only if pin PIO2_11/SCK0 selected in
Table 139)
it should say:
2:0 FUNC Selects pin function. All other values are reserved. 000
0x0 Selects function PIO2_11.
0x1 Selects function SCK0 (only if pin PIO2_11/SCK0 selected in
Table 139)
the right value is 1 and not 2