build openocd svn 2681 failed

Hello,

the bootstrap failed with the following errors:

aclocal-1.10

autoconf-2.63

Regards.

./bootstrap
+ aclocal
/usr/bin/m4:/tmp/am4t980WhI/traces.m4:2949: Warning: end of file treated as newline
+ libtoolize --automake --copy
+ autoconf
Use of uninitialized value in concatenation (.) or string at /usr/bin/autom4te-2.63 line 1024.
unknown channel m4trace at /usr/share/autoconf/Autom4te/Channels.pm line 546
        Autom4te::Channels::msg('m4trace', 'undef', 'warning: ') called at /usr/bin/autom4te-2.63 line 1024
Bootstrap complete; you can './configure --enable-maintainer-mode ....'

Hi,

It is working for me with the version

aclocal-1.11

autoconf-2.64

Update your design flow !

A trunk/testing/examples/LPC2148Test/makefile

U trunk

Checked out revision 2681.

done


  • Amontec Openocd Builder : COMPILING …

http:www.amontec.com

aclocal (GNU automake) 1.11

Copyright (C) 2009 Free Software Foundation, Inc.

License GPLv2+: GNU GPL version 2 or later <http://gnu.org/licenses/gpl-2.0.html

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.

Written by Tom Tromey <tromey@redhat.com>

and Alexandre Duret-Lutz <adl@gnu.org>.

libtoolize (GNU libtool 1.3110 2009-07-01) 2.2.7a

Written by Gary V. Vaughan <gary@gnu.org>, 2003

Copyright (C) 2009 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

autoconf (GNU Autoconf) 2.64

Copyright (C) 2009 Free Software Foundation, Inc.

License GPLv2+: GNU GPL version 2 or later

<http://gnu.org/licenses/old-licenses/gpl-2.0.html>

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.

Written by David J. MacKenzie and Akim Demaille.

autoheader (GNU Autoconf) 2.64

Copyright (C) 2009 Free Software Foundation, Inc.

License GPLv2+: GNU GPL version 2 or later

<http://gnu.org/licenses/old-licenses/gpl-2.0.html>

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.

Written by Roland McGrath and Akim Demaille.

automake (GNU automake) 1.11

Copyright (C) 2009 Free Software Foundation, Inc.

License GPLv2+: GNU GPL version 2 or later <http://gnu.org/licenses/gpl-2.0.html

This is free software: you are free to change and redistribute it.

There is NO WARRANTY, to the extent permitted by law.

Written by Tom Tromey <tromey@redhat.com>

and Alexandre Duret-Lutz <adl@gnu.org>.

GNU Make 3.81

Copyright (C) 2006 Free Software Foundation, Inc.

This is free software; see the source for copying conditions.

There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A

PARTICULAR PURPOSE.

regards,

Laurent

http://www.amontec.com

Amontec JTAGkey-2 : first High-Speed USB JTAG adapter 30Mhz TCK Frequency RTCK support 1.3V to 5.5V @ 32mA JTAG output driver 4 on-board leds for easy first use …