Can I borrow a hex file for the LPC1768?

Anyone? I just want a proven file - it can be designed to do anything…

I just need one that will pass the checks and vector off out of ISP and run. I’m in the middle of that classic ‘is it hardware or software?’ problem.

Unfortunately we’ve all been there.

Here is a hex file for an LPC1756 which will work on the 1768

It should print “Hi there %d” out UART0

and wiggle all the other ports

[

http://www.coridiumcorp.com/files/Xsample.hex

](http://www.coridiumcorp.com/files/Xsample.hex)

wooho That worked! Out of ISP and the LEDS are in a deterministic state. I’m sure I could drag it over to the scope now and see the heartbeat.

Now I just need to dig in and figure out the startup and linker stuff.

Thanks!!!

No possible way you could share that code and linker, hmmm?