djohnson:
It’s not that I’m lazy, it’s just just I can either design my PCB to have 12 resistors connecting to 12 LEDs (2 sets of 6), or 2 resistors connecting to each set. Fewer componets means less prone to error in my situation where soldering will be manual.
The LEDs belonging to each set are identical. Is there any reason why I still need a resistor for every LED?
Greetings djohnson et al.,
I’m here a little late - I see others have weighed in on the topic, which is a good one.
An LED is a diode (duh…) and has a non-linear impedance (resistance) depending upon the applied voltage. If the voltage is too low no current flows (expect some very small leakage current). As the voltage rises the current starts to flow - we’re on the knee of the diode’s VI curve. With little increase in voltage the LED (diode) draws ever greater current until the device is destroyed by self-heating.
The ballast resistor is used to limit the maximum current and prevent damage (or to set a lower current when less light is required for a given application). A particular diode has a knee voltage that varies with temperature, manufacturing tolerance (no two LEDs are the same), and LED construction (different colour LEDs have quite different voltages). Here’s a typical [high brighness LED data sheet.
LEDs have a negative temperature coefficient, meaning forward voltage decreases by about 20 mV for every 10° C rise in junction temperature. As noted by someone else, this could lead to a runaway failure of the LED.
Here’s an [LED app note on the topic.
If several LEDs are operated at the same time they may be placed in series - the same current flows through each one. The voltage across the string is the sum of the individuals and a single ballast resistor can be used to make up the difference from the supply voltage to the total of the LED voltages. Some LEDs in the string may be brighter for the given current (great effort is made for LED video screens to blance out the variations - sometimes you may see blotches of brightness variation or even a fixed rectangle that is out of adjustment).
If multiple LEDs are driven by DC and remain on at the same time, then a series string has the fewest components.
If multiple LEDs are not on at the same time, but driven by DC (via switches for example) they should have a separate resistor each.
A special case is if the LEDs are strobed (Multiplexed or MUX’d) above visual persistence (above 15 to 20 Hz) then a single resistor may serve mulitple LEDs. In this case each LED may be on for it’s time-slot, and the resistor is in play for just that LED. The LED will be off most of the time while the MUX driver services the other LEDs on the common resistor, so the current will fall to 1/n th the DC value. A smaller resistor is required to boost the LED current and bring up the brightness.
For example, if eight LEDs are MUX’d together, each LED is on for a max of 1/8th the time, so eight times the current must pass, and the resistor value is now 1/8th that required for DC operation of the same brightness. There is a practical limit to how many LEDs can be MUX’d as the on current must not exceed the abs. max. current for a given LED type.
In general modern LEDs are quite tough compared with the first examples - which stopped making light if you touched the leads for too long with a soldering iron.
Comments Welcome!](http://www.optekinc.com/pdf/AppNote228.pdf)](http://www.optekinc.com/pdf/ovfsrac8.pdf)