trying to go through all the doc i can find on this board and am not 100% certain on whether or not i can power this from a cars 12v electrical system. And if i do have it hardwired and mounted in a car how does this affect programming while running off of the cars power ?
The barrel jack is where you supply power. Alternatively, you can use the nearby VIN and GND via’s for supplying power. Either way, any input voltage between 6V and 15V will work.
- If you’re planning to use the on-board amplifier, read this first. Next, please consider using a
supply voltage of no more than 9V, preferably less. Playing loud audio with the on-board amp for
extended periods can draw a lot of current and the lower the input voltage, the less warm the 5V
regulator will get. This is especially important if you’re encasing the WAV Trigger in a small
project box. I personally use 6V wall mount adaptors like this. Alternatively, you can power the
WAV Trigger with regulated 5V (5Vin) and bypass the on-board regulator completely