hello!
I have conected the em-406 to my sparkfun gps eval.board and resive signals when I use sirfdemo and quickterm dt.but once I`ve hook it up on my gps shield on top of my arduino and run the gps test parsing sketch from ladyada I dont resive anything. The em-406 is blinking so its working but the tx and rx lights on my arduino are not active.Iknow I have to set the button on the gps shield to dline to transfer the program to arduino.I have tried to set it in uart posision as well but still not working.The arduino program just says:
GPS parser
read:
Do I have to connect the tx and rx on the arduino to the gps shield with jumpers?
I thought it was enough to solder the 6 and 8 pins to the gps shield and insert it on top of the arduino board ![]()
greatings from Norway ![]()