Can Wixel be used to communicate with CC2500?

I searching for a good/reliable RF CC2500 transmitter.

Can the Wixel be used to send data to a CC2500 client?

I’ve tried a Chinese CC2500 (actually a XL2500) as host but have trouble keeping steady communication.

It’s a bit strange, it’s not a range issue: it sometimes works 30 feet away and yet fails a few feet away and seems to be very location-dependent.

I know the CC2511 chip can do CC2500 communication but I’m not sure if the “Wixel” has been programmed with it’s own protocol so that it is not compatible with a generic CC2500.

I can’t make changes to the client aside from what the sender can negotiate.

Some of the the CC2500 client params:

IF frequency of 253.9kHz

FREQ = 2420 MHz

CHANBW = 541.666 kHz

DRATE = 249.94 kBaud

MSK modulation, 30/32 sync word bits

FEC disabled,

2 preamble bytes

CHANSPC = 199.951 kHz

CHANNEL = 1

If the answer is yes, can the Wixel be outfitted with an external antenna to increase range?

A better place to post would be the Polulu Wixel forum.

Thanks for pointing me to Polulu.

I just discovered the Wixel, and now I discover Polulu.

From their “FAQ” it seems to be possible, at least they do mention the CC2500. Still wondering if I can manipulate the protocol but I asked more specific question to that effect in their Wixel forum.