Can't program LoRa board

Board: WRT-14916

Arduino Version: 1.8.13

Mac OSX 11.0.1

I can select the board from the board menu and the board shows up under port at the Pro RF board. When I try to program the board, I get the following error:

java.io.IOException: Cannot run program "{runtime.tools.bossac-1.7.0-arduino3.path}/bossac": error=2, No such file or directory
	at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
	at java.lang.Runtime.exec(Runtime.java:620)
	at java.lang.Runtime.exec(Runtime.java:485)
	at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:11)
	at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:129)
	at cc.arduino.packages.uploaders.SerialUploader.runCommand(SerialUploader.java:383)
	at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:197)
	at cc.arduino.UploaderUtils.upload(UploaderUtils.java:77)
	at processing.app.SketchController.upload(SketchController.java:732)
	at processing.app.SketchController.exportApplet(SketchController.java:703)
	at processing.app.Editor$UploadHandler.run(Editor.java:2055)
	at java.lang.Thread.run(Thread.java:748)
Caused by: java.io.IOException: error=2, No such file or directory
	at java.lang.UNIXProcess.forkAndExec(Native Method)
	at java.lang.UNIXProcess.<init>(UNIXProcess.java:247)
	at java.lang.ProcessImpl.start(ProcessImpl.java:134)
	at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
	... 11 more
An error occurred while uploading the sketch

It looks like the build system is trying to use the 1.7 version of the Arduino tools instead of 1.8. Any idea how to fix this?

Thanks,

Rob

I was able to solve this by uninstalling Arduino and the Arduino Libraries and re-installing them.