I’m using Sparkfun’s SEN-08554 IR receiver and remote to control a clock that I’m making. However, I’m having a little trouble implementing the code for the IR receiver.
I’m using Ken Sherriff’s library and the code that Sparkfun provided:
#include <IRremote.h>
int RECV_PIN = 46; //pin 46 for the Mega2560
IRrecv irrecv(RECV_PIN);
decode_results results;
#define A 0x10EFF807
void setup()
{
  Serial.begin(115200);
  irrecv.enableIRIn(); // Start the receiver
}
void loop() 
{
  if (irrecv.decode(&results)) 
  {
    if (results.value == A) 
    {
      Serial.println("A");    
    }
    irrecv.resume();
  }
}
For the ease of reading, I trimmed the code down to just the one “A” button, but all buttons are in the code. Running that code on my Mega works great. So all the hardware is fine. It’s when I add it to my clock sketch that the problems arise.
What I’m trying to do is display my clock code in the main loop (time and date displayed from a DS3231 RTC), and then bring up a settings menu with a button press on the remote. It doesn’t seem to work.
What I’d like is for the menu function to be called when button “A” is pressed, but otherwise run the rest of the code in my main loop:
void loop() 
{
  if (irrecv.decode(&results)) 
  {
    if (results.value == A) 
    {
      Serial.println("A");  
	buttonAPressed():  //call this function when “A” is pressed
    }
    irrecv.resume();
  }
//no IR codes rec’d, continue displaying main clock display
	//regular clock display code goes here
	//blah
	//blah
	//blah
}
void buttonAPressed {
//display settings menu
	//blah
	//blah
	//blah
}
However, if I do it like that, my clock code/display shows fine, but buttonAPressed is never called. I can’t figure out why.
If I place my clock display code within “if (irrecv.decode(&results))”, the remote works, but the clock display code is only displayed when a button is pressed. I need that code to run when nothing is pressed! It’s like I get what’s either in “if (irrecv.decode(&results))” or the main loop, but not both.
void loop() 
{
  if (irrecv.decode(&results)) 
  {
    if (results.value == A) 
    {
      Serial.println("A");  
	buttonAPressed():  
    }
    irrecv.resume();
  
//regular clock display code here
//blah
//blah
//blah
 }
}
void buttonAPressed {
//display settings menu
	//blah
	//blah
	//blah
}
I’ve tried sticking “irrecv.resume();” in various places, but it doesn’t seem to make a difference.
I even tried handling the remote in a separate function like this
void loop() {
  if (irrecv.decode(&results))   {
    handleRemote(&results):  //I think I pass "&results" here?
    }
    irrecv.resume();
  }
//regular clock display code here
//blah
//blah
//blah
 }
void handleRemote() { //or is it void handleRemote(&results)? I think I tried various things without success
if (results.value == A) 
    {
      Serial.println("A");  
	buttonAPressed():  
    }
}
But that still doesn’t get called. What am I doing wrong? I’ve been at this for days and I just can’t get the loop to run as normal, but step into another function when a button is pressed.
Here’s my full sketch will everything:
#include <Adafruit_GPS.h>
#include <SoftwareSerial.h>
#include <Wire.h>
#include <DS3231.h>
#include <glcd.h>
#include <fonts/SystemFont5x7.h>
#include <fonts/Arial14.h>             
#include <fonts/Arial_bold_14.h>       
#include <fonts/fixednums7x15.h>       
#include <fonts/fixednums8x16.h>
#include <fonts/fixednums15x31.h>
#include <IRremote.h>
DS3231 RTC; //Create the DS3231 object
//remote
int RECV_PIN = 46; //pin 46 is for the Mega per Timer5 in the IR library
IRrecv irrecv(RECV_PIN);
decode_results results;
#define POWER 0x10EFD827 
#define A 0x10EFF807 
#define B 0x10EF7887
#define C 0x10EF58A7
#define UP 0x10EFA05F
#define DOWN 0x10EF00FF
#define LEFT 0x10EF10EF
#define RIGHT 0x10EF807F
#define SELECT 0x10EF20DF
//temp
int tempC;
int tempF;
//initial condition for menu display
boolean enterNormalMode = true;
boolean enterSettingsMode = false;
boolean enterAlarmMode = false;
boolean chimeOnHour = false;
boolean alarmIsActive = false;
//settings menu
int settingsModeButtonCount;
boolean gmtSelected = false;
boolean dlsSelected = false;
boolean chimeSelected = false;
//alarm menu
int alarmModeButtonCount;
boolean aTimeSelected = false;
boolean activeSelected = false;
//compensations
int TZAdjust; 
int newHours;
int DaylightSavings;
boolean DLSinEffect = false;
//year, month, date, hour, min, sec and week-day(starts from 0 and goes to 6)
//writing any non-existent time-data may interfere with normal operation of the RTC.
//Take care of week-day also.
//DateTime dt(2013, 11, 2, 22, 03, 00, 6);
int hhRTC;
int hhAdj;
int mmRTC;
int ssRTC;
int dayRTC;
int dowRTC;
int monthRTC;
int yearRTC;
int hhGPS;
int newHourGPS;
int mmGPS;
int ssGPS;
int dayGPS;
int monthGPS;
int yearGPS;
int linkStatus;
// If you're using a GPS module:
// Connect the GPS Power pin to 5V
// Connect the GPS Ground pin to ground
// If using software serial (sketch example default):
//   Connect the GPS TX (transmit) pin to Digital 3
//   Connect the GPS RX (receive) pin to Digital 2
// If using hardware serial (e.g. Arduino Mega):
//   Connect the GPS TX (transmit) pin to Arduino RX1, RX2 or RX3
//   Connect the GPS RX (receive) pin to matching TX1, TX2 or TX3
// If you're using the Adafruit GPS shield, change 
// SoftwareSerial mySerial(3, 2); -> SoftwareSerial mySerial(8, 7);
// and make sure the switch is set to SoftSerial
// If using software serial, keep these lines enabled
// (you can change the pin numbers to match your wiring):
//SoftwareSerial mySerial(3, 2);
//Adafruit_GPS GPS(&mySerial);
// If using hardware serial (e.g. Arduino Mega), comment
// out the above six lines and enable this line instead:
Adafruit_GPS GPS(&Serial1);
// Set GPSECHO to 'false' to turn off echoing the GPS data to the Serial console
// Set to 'true' if you want to debug and listen to the raw GPS sentences. 
#define GPSECHO  true
// this keeps track of whether we're using the interrupt
// off by default!
boolean usingInterrupt = false;
void useInterrupt(boolean); // Func prototype keeps Arduino 0023 happy
int enablePin = 7;
void setup()  
{
  pinMode(enablePin, OUTPUT);
  digitalWrite(enablePin, HIGH); //enable GPS
  // connect at 115200 so we can read the GPS fast enough and echo without dropping chars
  // also spit it out
  Serial.begin(115200);
  Serial.println("Adafruit GPS library basic test!");
  // 9600 NMEA is the default baud rate for Adafruit MTK GPS's- some use 4800
  GPS.begin(9600);
  // uncomment this line to turn on RMC (recommended minimum) and GGA (fix data) including altitude
  GPS.sendCommand(PMTK_SET_NMEA_OUTPUT_RMCGGA);
  // uncomment this line to turn on only the "minimum recommended" data
  //GPS.sendCommand(PMTK_SET_NMEA_OUTPUT_RMCONLY);
  // For parsing data, we don't suggest using anything but either RMC only or RMC+GGA since
  // the parser doesn't care about other sentences at this time
  // Set the update rate
  GPS.sendCommand(PMTK_SET_NMEA_UPDATE_1HZ);   // 1 Hz update rate
  // For the parsing code to work nicely and have time to sort thru the data, and
  // print it out we don't suggest using anything higher than 1 Hz
  // Request updates on antenna status, comment out to keep quiet
  GPS.sendCommand(PGCMD_ANTENNA);
  // the nice thing about this code is you can have a timer0 interrupt go off
  // every 1 millisecond, and read data from the GPS for you. that makes the
  // loop code a heck of a lot easier!
  useInterrupt(true);
  delay(1000);
  // Ask for firmware version
  // mySerial.println(PMTK_Q_RELEASE);
  digitalWrite(enablePin, LOW); //disable GPS
  // Initialize the GLCD 
  GLCD.Init();
  Wire.begin(); //I think enabeling the wire library casues the problem
  RTC.begin();
  irrecv.enableIRIn(); // Start the IR receiver
  //unhide to force time setting of the RTC
  // RTC.adjust(dt); //Adjust date-time as defined 'dt' above 
}
// Interrupt is called once a millisecond, looks for any new GPS data, and stores it
SIGNAL(TIMER0_COMPA_vect) {
  char c = GPS.read();
  // if you want to debug, this is a good time to do it!
#ifdef UDR0
  if (GPSECHO)
    if (c) UDR0 = c;  
  // writing direct to UDR0 is much much faster than Serial.print 
  // but only one character can be written at a time. 
#endif
}
void useInterrupt(boolean v) {
  if (v) {
    // Timer0 is already used for millis() - we'll just interrupt somewhere
    // in the middle and call the "Compare A" function above
    OCR0A = 0xAF;
    TIMSK0 |= _BV(OCIE0A);
    usingInterrupt = true;
  } 
  else {
    // do not call the interrupt function COMPA anymore
    TIMSK0 &= ~_BV(OCIE0A);
    usingInterrupt = false;
  }
}
void loop() {
  //remote
  if (irrecv.decode(&results)) {
    if (results.value == POWER) 
    {
      Serial.println("POWER");  
      syncGPSTime();  
    }
    if (results.value == A) 
    {
      Serial.println("A");  
      buttonAPressed();
    }
    if (results.value == B) 
    {
      Serial.println("B"); 
      buttonBPressed();
    }
    if (results.value == C) 
    {
      Serial.println("C");
      buttonCPressed();
    }
    if (results.value == UP) 
    {
      Serial.println("UP");
      buttonUPPressed();
    }
    if (results.value == DOWN) 
    {
      Serial.println("DOWN");
      buttonDownPressed();      
    }
    if (results.value == LEFT) 
    {
      Serial.println("LEFT");
      buttonLeftPressed();
    }
    if (results.value == RIGHT) 
    {
      Serial.println("RIGHT");
      buttonRightPressed();
    }
    if (results.value == SELECT) 
    {
      Serial.println("SELECT");  
      buttonSelectPressed();
    }
    irrecv.resume();
  }
  //////////////////////////////////////////////////////////////
  //RTC
  DateTime now = RTC.now();
  tempC = RTC.getTemperature();
  tempF = (tempC * 9.0)/ 5.0 + 32.0; // Convert C to F
  hhRTC = now.hour(); //used to check AM/PM status
  mmRTC = now.minute();
  ssRTC = now.second(); 
  dowRTC = now.dayOfWeek();
  dayRTC = now.date();
  monthRTC = now.month();
  yearRTC = now.year();
  //pass RTC values into a new variable -
  //this way one variable stores time in 24 hour mode and another that can be converted to 12 hour mode
  //time is monitored 'in the background' in 24 hour mode using the RTC, but is displayed in an adjusted 12-hr format
  hhAdj = hhRTC;
  //convert to 12 hr mode for display
  if (hhRTC < 1) {
    hhAdj = 12;
  }
  if ((hhRTC > 12) && (hhRTC < 24)) {
    hhAdj = hhRTC - 12;
  }
  //DLS compensation
  if (DLSinEffect == false) {
    DaylightSavings = 0; //DSL not in effect, don't add an additional hour
  } 
  else {
    DaylightSavings = 1; //DSL in effect, add an additional hour
  }
  newHours = ((hhAdj) + TZAdjust + DaylightSavings);
  ////////////////////////////////////////////////////////////////////////////////
  //not in menu mode
  //time from RTC
  if (enterNormalMode == true) {
    //hour
    GLCD.SelectFont(fixednums15x31);
    GLCD.CursorTo(0,0);
    if (newHours < 10) {
      GLCD.print("0"); 
    } 
    GLCD.print(newHours);
    //minute
    if (mmRTC < 10) {
      GLCD.print(":0"); 
    } 
    else {
      GLCD.print(":");
    }
    GLCD.print(mmRTC);
    //second
    GLCD.SelectFont(fixednums7x15);
    if (ssRTC < 10) {
      GLCD.print(":0"); 
    } 
    else {
      GLCD.print(":");
    }
    GLCD.print(ssRTC);
    // AM/PM indicator
    GLCD.SelectFont(SystemFont5x7);
    if ((hhRTC > 12) && (hhRTC < 22)) {
      //PM
      GLCD.print(" PM");
    } 
    else {
      //AM
      GLCD.print(" AM"); 
    }
    //second line
    //date
    GLCD.CursorTo(0,4);
    GLCD.SelectFont(Arial14);
    switch(dowRTC){
    case 0: 
      GLCD.print("Sun  ");
      break;
    case 1: 
      GLCD.print("Mon  ");
      break;
    case 2: 
      GLCD.print("Tue  ");
      break;
    case 3: 
      GLCD.print("Wed  ");
      break;
    case 4: 
      GLCD.print("Thu  ");
      break;
    case 5: 
      GLCD.print("Fri  ");
      break;
    case 6: 
      GLCD.print("Sat  ");
      break;
    }
    GLCD.SelectFont(fixednums7x15);
    GLCD.print(monthRTC);
    GLCD.print("/");
    GLCD.print(dayRTC);
    GLCD.print("/");
    GLCD.print(yearRTC - 2000);
    //temp
    GLCD.SelectFont(SystemFont5x7);
    GLCD.print("  ");
    GLCD.SelectFont(fixednums8x16);
    GLCD.print(tempF);
    GLCD.SelectFont(SystemFont5x7);
    GLCD.print("F"); 
    //draw line
    GLCD.DrawLine(0,51,128,51,BLACK);
    //GPS status
    linkStatus = (GPS.fixquality);
    GLCD.SelectFont(SystemFont5x7);
    GLCD.CursorTo(0,7);
    if (linkStatus < 1) {
      GLCD.print("GPS:NO ");
    } 
    else {
      GLCD.print("GPS:YES");
    }
    //alarm
    GLCD.print("  ALARM:");
    if (alarmIsActive == true) {
      GLCD.print("6:30AM");
    } 
    else {
      GLCD.print("OFF");
    }
  }
  ////////////////////////////////////////////////////////////////////////////////
  //display settings menu
  if (enterSettingsMode == true) {
    GLCD.ClearScreen();
    //settings menu header
    GLCD.SelectFont(SystemFont5x7);
    GLCD.CursorTo(0,0);
    GLCD.print("     "); 
    GLCD.SelectFont(Arial_bold_14);
    GLCD.print("SETTINGS"); 
    //draw line
    GLCD.DrawLine(0,12,128,12,BLACK);
    if (settingsModeButtonCount == 3) { //no option highlighted
      gmtSelected = false;
      dlsSelected = false;
      chimeSelected = false;
      GLCD.SelectFont(Arial14);
      //time zone
      GLCD.CursorTo(0,1);
      GLCD.print("GMT:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      GLCD.print(TZAdjust); 
      //daylight savings 
      GLCD.CursorTo(0,2);
      GLCD.print("DLS:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (DLSinEffect == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
      //chime on hour
      GLCD.CursorTo(0,3);
      GLCD.print("CHIME:");
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (chimeOnHour == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    if (settingsModeButtonCount == 2) { //GMT highlighted
      gmtSelected = true;
      dlsSelected = false;
      chimeSelected = false;
      GLCD.SelectFont(Arial_bold_14);
      //time zone
      GLCD.CursorTo(0,1);
      GLCD.print("GMT:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial_bold_14);
      GLCD.print(TZAdjust); 
      GLCD.SelectFont(Arial14);
      //daylight savings 
      GLCD.CursorTo(0,2);
      GLCD.print("DLS:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (DLSinEffect == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      } 
      //chime on hour
      GLCD.CursorTo(0,3);
      GLCD.print("CHIME:");
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (chimeOnHour == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    if (settingsModeButtonCount == 1) { //DLS highlighted
      gmtSelected = false;
      dlsSelected = true;
      chimeSelected = false;
      GLCD.SelectFont(Arial14);
      //time zone
      GLCD.CursorTo(0,1);
      GLCD.print("GMT:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      GLCD.print(TZAdjust); 
      GLCD.SelectFont(Arial_bold_14);
      //daylight savings 
      GLCD.CursorTo(0,2);
      GLCD.print("DLS:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial_bold_14);
      if (DLSinEffect == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
      //chime on hour
      GLCD.SelectFont(Arial14);
      GLCD.CursorTo(0,3);
      GLCD.print("CHIME:");
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (chimeOnHour == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    if (settingsModeButtonCount == 0) { //CHIME highlighted
      gmtSelected = false;
      dlsSelected = false;
      chimeSelected = true;
      GLCD.SelectFont(Arial14);
      //time zone
      GLCD.CursorTo(0,1);
      GLCD.print("GMT:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      GLCD.print(TZAdjust); 
      //daylight savings 
      GLCD.CursorTo(0,2);
      GLCD.print("DLS:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (DLSinEffect == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
      //chime on hour
      GLCD.SelectFont(Arial_bold_14);
      GLCD.CursorTo(0,3);
      GLCD.print("CHIME:");
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial_bold_14);
      if (chimeOnHour == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    //add delay to lower refresh rate on the display (remove blink)
    delay(200);
  }
  ////////////////////////////////////////////////////////////////////////////////
  //display alarm menu
  if (enterAlarmMode == true) {
    GLCD.ClearScreen();
    //settings menu header
    GLCD.SelectFont(SystemFont5x7);
    GLCD.CursorTo(0,0);
    GLCD.print("     "); 
    GLCD.SelectFont(Arial_bold_14);
    GLCD.print("  ALARM"); 
    //draw line
    GLCD.DrawLine(0,12,128,12,BLACK);
    if (alarmModeButtonCount == 2) {//no option highlighted
      aTimeSelected = false;
      activeSelected = false;
      GLCD.SelectFont(Arial14);
      //alarm
      GLCD.CursorTo(0,1);
      GLCD.print("TIME:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      GLCD.print("6:30 AM"); 
      //alarm status
      GLCD.CursorTo(0,2);
      GLCD.print("ACTIVE:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (alarmIsActive == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    if (alarmModeButtonCount == 1) {//TIME option highlighted
      aTimeSelected = true;
      activeSelected = false;
      GLCD.SelectFont(Arial14);
      //alarm
      GLCD.CursorTo(0,1);
      GLCD.SelectFont(Arial_bold_14);
      GLCD.print("TIME:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial_bold_14);
      GLCD.print("6:30 AM"); 
      //alarm status
      GLCD.CursorTo(0,2);
      GLCD.SelectFont(Arial14);
      GLCD.print("ACTIVE:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      if (alarmIsActive == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    if (alarmModeButtonCount == 0) {//ALARM option highlighted
      aTimeSelected = false;
      activeSelected = true;
      GLCD.SelectFont(Arial14);
      //alarm
      GLCD.CursorTo(0,1);
      GLCD.SelectFont(Arial14);
      GLCD.print("TIME:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial14);
      GLCD.print("6:30 AM"); 
      //alarm status
      GLCD.CursorTo(0,2);
      GLCD.SelectFont(Arial_bold_14);
      GLCD.print("ACTIVE:"); 
      GLCD.SelectFont(SystemFont5x7);
      GLCD.print(" "); 
      GLCD.SelectFont(Arial_bold_14);
      if (alarmIsActive == true) {
        GLCD.print("YES");
      } 
      else {
        GLCD.print("NO");
      }
    }
    //add delay to lower refresh rate on the display (remove blink)
    delay(200);
  }
} //end of loop
//////////////////////////////////////////////////////////////
//remote functions
//GPS
void syncGPSTime() {
  digitalWrite(enablePin, HIGH);
  // if a sentence is received, we can check the checksum, parse it...
  if (GPS.newNMEAreceived()) {
    // a tricky thing here is if we print the NMEA sentence, or data
    // we end up not listening and catching other sentences! 
    // so be very wary if using OUTPUT_ALLDATA and trytng to print out data
    //Serial.println(GPS.lastNMEA());   // this also sets the newNMEAreceived() flag to false
    if (!GPS.parse(GPS.lastNMEA()))   // this also sets the newNMEAreceived() flag to false
      return;  // we can fail to parse a sentence in which case we should just wait for another
  }
  Serial.print("\nTime: ");
  Serial.print(GPS.hour, DEC); 
  Serial.print(':');
  Serial.print(GPS.minute, DEC); 
  Serial.print(':');
  Serial.print(GPS.seconds, DEC); 
  Serial.print('.');
  Serial.println(GPS.milliseconds);
  Serial.print("Date: ");
  Serial.print(GPS.day, DEC); 
  Serial.print('/');
  Serial.print(GPS.month, DEC); 
  Serial.print("/20");
  Serial.println(GPS.year, DEC);
  Serial.print("Fix: "); 
  Serial.print((int)GPS.fix);
  Serial.print(" quality: "); 
  Serial.println((int)GPS.fixquality); 
  if (GPS.fix) {
    Serial.print("Location: ");
    Serial.print(GPS.latitude, 4); 
    Serial.print(GPS.lat);
    Serial.print(", "); 
    Serial.print(GPS.longitude, 4); 
    Serial.println(GPS.lon);
    Serial.print("Speed (knots): "); 
    Serial.println(GPS.speed);
    Serial.print("Angle: "); 
    Serial.println(GPS.angle);
    Serial.print("Altitude: "); 
    Serial.println(GPS.altitude);
    Serial.print("Satellites: "); 
    Serial.println((int)GPS.satellites);
  }
newHourGPS = ((hhGPS) + TZAdjust + DaylightSavings);
//day of week is hard coded until a calculation can be added
//can I get this from the Time library?
//http://playground.arduino.cc/Code/Time
DateTime dt(yearGPS, monthGPS, dayGPS, newHourGPS, mmGPS, ssGPS, 6);
  
  //add compensation here
  //do not force update if data is invalid
  //
  //
  
  RTC.adjust(dt); 
  delay(10);
  GLCD.ClearScreen();
  
 //turn off GPS module
 digitalWrite(enablePin, LOW);
}
//A
void buttonAPressed() {
  enterNormalMode = true;
  enterSettingsMode = false;
  enterAlarmMode = false;
  GLCD.ClearScreen();
}
//B
void buttonBPressed() {
  //enter menu in default state so no options are highlighted
  settingsModeButtonCount = 3; 
  enterNormalMode = false;
  enterSettingsMode = true;
  enterAlarmMode = false;
  GLCD.ClearScreen();
}
//C
void buttonCPressed() {
  //enter menu in default state so no options are highlighted
  alarmModeButtonCount = 2;
  enterNormalMode = false;
  enterSettingsMode = false;
  enterAlarmMode = true;
  GLCD.ClearScreen();
}
//UP
void buttonUPPressed() {
  if(enterSettingsMode == true) {
    settingsModeButtonCount++;
    if(settingsModeButtonCount == 4) { 
      settingsModeButtonCount = 0;
    }
  }
  if(enterAlarmMode == true) {
    alarmModeButtonCount++;
    if(alarmModeButtonCount == 3) {
      alarmModeButtonCount = 0;
    }
  }
}
//DOWN
void buttonDownPressed() {
  if(enterSettingsMode == true) {
    settingsModeButtonCount--;
    if(settingsModeButtonCount < 0) {
      settingsModeButtonCount = 3;
    }
  }
  if(enterAlarmMode == true) {
    alarmModeButtonCount--;
    if(alarmModeButtonCount < 0) {
      alarmModeButtonCount = 2;
    }
  }
}
//LEFT
void buttonLeftPressed() {
  if(gmtSelected == true) {
    TZAdjust--;
    //time zone changed - resync with GPS clock
    syncGPSTime();
  }
  if(dlsSelected == true) {
    DLSinEffect = !DLSinEffect;
  }
  if(chimeSelected == true) {
    chimeOnHour = !chimeOnHour;
  }
  if(aTimeSelected == true) {
  }
  if(activeSelected == true) {
    alarmIsActive = !alarmIsActive;
  }
}
//RIGHT
void buttonRightPressed() {
  if(gmtSelected == true) {
    TZAdjust++;
    //time zone changed - resync with GPS clock
    syncGPSTime();
  }
  if(dlsSelected == true) {
    DLSinEffect = !DLSinEffect;
  }
  if(chimeSelected == true) {
    chimeOnHour = !chimeOnHour;
  }
  if(aTimeSelected == true) {
  }
  if(activeSelected == true) {
    alarmIsActive = !alarmIsActive;
  }
}
//SELECT
void buttonSelectPressed() {
  //set totally wrong date and time (so that a GPS sync can be tested)
  DateTime dt(2011, 1, 1, 1, 1, 0, 6);
  RTC.adjust(dt); 
  delay(10);
  GLCD.ClearScreen();
}