Choosing solder types?

Hi there,

The following are some of types of solder that I have heard of.

My question is: How to choose which one for a particular job? I mean why there are different types (apart from lead free)? Is each type designed for a particular applications?

The bottomline: how to choose one for just general PCB soldering?

85Sn/15Pb

70 Sn/30Pb

63Sn/37Pb

60 Sn/40Pb

Sn/Ag3.5

Sn/Cu 75

Sn/Ag4.0/Cu.5

Sn/Ag2.5/Cu.8/Sb.5

Sn/Bi3.0/Ag3.0

60/40 Sn/Pb is usual for lead solder. Multticore with rosin flux is best for general use, but the flux should be removed soon after soldering as it becomes difficult to remove if left on boards.

Leon

For leaded boards, I use 63/37 (eutectic) solder. For unleaded, I just curse.

Most people choose solder based on one of two factors.

  1. Liquidous temperature (temperature the solder turns liquid)

  2. Strength

60sn/40pb probably has the lowest melting temperature of all solders.

63sn/37pb is nice because it melts uniformly

85sn/15pb is a harder solder because of the lower lead content and has better electrical properties

Most solder requirements for production are centered around reflow temperature (or wave) and electrical requirements. Higher silver content has better electrical properties.

There is a science behind solder, but most designs do not require a in-depth research of the required solder. Most are pushed toward the lower temperatures because of the IC’s used (in lead free any way).

There are other items not listed here with regards to flux/rosin.

James L