Wow…
First off- let me say thank you to all that have replied with suggestions.
Secondly - I made a mistake on the fritzing image relating to wiring of the regulator - you were right Mee-n-Mac - I showed it incorrectly wired on the dwg - but on the breadboard - I wired it correctly and verified 3.3v output.
@waltr - I don’t know how to determine the Peak Current Draw of the motor. But I just measured the resistance at 32.6 ohms.
I can answer most of the questions I think by explaining more about the motor…
I purchased a 12v Door lock from ebay (cheap import).
It has a small electric motor in it that cycles an actuator in one direction, then if you reverse the polarity it reverses the direction. Pushing and pulling the actuator.
I discovered at the expense of my first mosfet, when I put a spring (rubber band) on the actuator - that when it cycled back to the extended position - the motor was no longer a motor and became a generator - producing voltage (around 1.6v) - which I believe ran back thru the neg wire and fried the NMOSFET ( https://www.sparkfun.com/products/10213 ). According to the specs @ SF the NMOSFET is supposed to cycle full on with as little as 3v, which is why I was using it on the Rx signal leg of the BlueTooth transceiver.
I was originally doing all of this development using a 12v wallwart (from SF) - It’s likely I ruined more than one device by trying to check voltage across terminals and legs of the circuit with my low end DVM.
I was hoping that I could cycle the actuator (motor) using a 3v feed from the BlueTooth device by turning the NMOSFET on and (originally) sending 12v to the motor / actuator. I’ve since discovered the actuator works fine on 5v.
I couldn’t find a reference in fritzing to a 5v source - so I threw a 9v battery on the diagram - close enough?
In order to try to protect the NMOSFET and do something with the energy produced by the motor when cycled back to extended position - I put a diode between the leads to the motor - and an LED to help dissipate the energy being generated by the return of the actuator to the extended position (rubber band / generator).
I’m not positive - but I believe that worked briefly, the signal from the BT device cycled the NMOSFET - which completed the circuit to the motor - The LED would glow brightly for a fraction of a second. But I noticed during some cycles the red SMD led on the bluetooth device went out after each cycle of the actuator - which I also believe eventually damaged the bluetooth device, as both the Tx and Rx legs stopped working (no voltage output).
Which lead me to believe there’s more stray voltage running around after an actuator cycle and I needed to add more diodes to snub the stray voltage and try to prevent it from backflowing to the other elements of the circuit.
After damaging all my spare NMOSFETS (3v would no longer enable the switch), I tried a transistor - which resulted in lots of smoke and a small blister on the end of my index finger.
So… I ordered more parts, revised the schematic by putting diodes (1 way valves) everywhere I thought there might be a path for stray voltage, and then came here for help - which I really appreciate BTW.
Regarding the Rx / Tx connection - you may be right Mee -n- Mac - I was thinking the rx leg would go high when the receiver got a message from the phone - but it could be the other way around. I noticed the Tx leg was pulsing continuously regardless of initial connection - so It could be I’ve got the circuit backwards - I’ll need to get more info from the manufacturer to understand that - It may not be possible to do what I want with this device …
Thanks again for all the help - maybe the explanation above will help with understanding what may have gone wrong and result in a workable (better) design.
I removed most of the diodes referenced and added a 10uF capacitor to the output of the regulator and revised the schematic. After reading this hopefully someone can suggest where the diodes need to be placed to protect the transceiver from stray voltage. At the suggestion of other boards - I have a 10k pulldown resistor on the gate leg of the NMOSFET.
Revised schematic:(click for larger image)
[
](http://www.bnite.com/GPMotor_bbV3L.png)