CircuitPython Support for MicroMod STM32 - need USB PID

I’m working on adding support for the [MicroMod STM32 board to CircuitPython in https://github.com/adafruit/circuitpython/pull/5060. I need an official USB PID for the board from Sparkfun before the PR can be finalized. Could someone from SparkFun post a reply in the github PR with the correct USB VID/PID I should use for this board?](SparkFun MicroMod STM32 Processor - DEV-17713 - SparkFun Electronics)

Thanks for reaching out! I checked our in-house wiki to see if that particular PID was posted yet, it isn’t :frowning:

The engineers are much more active on github, which is likely where they’ll be responding to this request.

Thanks for contributing!

Update

PID: 0x0027

VID: 0X1B4F

Off to the races!

Thank you! PR is now updated with the new PID.

@Cdwilson

Looks like there may have been some confusion or some background changes that were not communicated. The correct PID for the MicroMod STM32 processor is 0x0029.

@TheHoff @TS-Russell Apologies, I missed this reply from the old forum.

FYI, I’ve created a PR to use the correct PID:

Can you double check the PR to confirm it’s correct?

Looks good to me!