Code obstacle avoider+ir remote+HC05 bluetooth mobile controller+line follower

I am trying to make an obstacle avoider with ir remote controller with HC05 bluetooth mobile controller with line follower ! But unfortunately I’m not able to get an perfect code for these particular functions… Im just an starter with programming.

If any one woud be able to help me then please do!!

Thanks in advance

https://i.stack.imgur.com/9zS17.jpg wiring diagram

https://i.stack.imgur.com/Qr7rO.jpg Components

This is the code I tried to use

//====================================================================

// Comprehensive Experiment

//=============================================================================

#include “./IRremote.h”

//Infrared Remote Control

//==============================

int RECV_PIN = 2; // Set Infrared Remote port

IRrecv irrecv(RECV_PIN);

decode_results results; // Store infrared remote decode data

unsigned long last = millis();

#define run_car ‘1’//key go

#define back_car ‘2’//key back

#define left_car ‘3’//key left

#define right_car ‘4’//key right

#define stop_car ‘0’//key stop

//===============================================

/Car running status enumeration/

//============================================

enum {

enSTOP = 0,

enRUN,

enBACK,

enLEFT,

enRIGHT,

enTLEFT,

enTRIGHT

} enCarState;

//==============================

//==============================

//Speed control

//==============================

int control = 150;//PWM control speed

#define level1 0x08//Speed level flag

#define level2 0x09

#define level3 0x0A

#define level4 0x0B

#define level5 0x0C

#define level6 0x0D

#define level7 0x0E

#define level8 0x0F

//==============================

//==============================

int Left_motor_back=9;

int Left_motor_go=8;

int Right_motor_go=6;

int Right_motor_back=7;

int Right_motor_en=5;

int Left_motor_en=10;

//==============================

//Bluetooth protocol related

//==============================

int incomingByte = 0; // Store Received Data(byte)

String inputString = “”; // Store Received Data(String)

boolean newLineReceived = false; // Previous data end flag

boolean startBit = false; // Protocol start flag

String returntemp = “”; // Store return data

/Set BUZZER port/

int BUZZER = 12;

/Set Button port/

int KEY = 13;

/Set right &left LED port/

int right_led=4;

int left_led=3;

/Set Ultrasonic Sensor/

int Echo = A1; // Set Echo port

int Trig = A0; // Set Trig port

int Distance = 0;

/Line Walking/

const int SensorRight = A2; // Set Right Line Walking Infrared sensor port

const int SensorLeft = A3; // Set Left Line Walking Infrared sensor port

int SL; // State of Left Line Walking Infrared sensor

int SR; // State of Right Line Walking Infrared sensor

/follow/

const int SensorRight_2 = A4; // Right Tracking Infrared sensor

const int SensorLeft_2 = A5; // Left Tracking Infrared sensor

int SL_2; // State of Left Tracking Infrared sensor

int SR_2; // State of Right Tracking Infrared sensor

//State

int g_carstate = enSTOP; // 1:front 2:back 3:left 4:right 0:stop // State of vehicle running state

int g_modeSelect = 0; // 0:remote control mode(default); 1:line walking mode ; 2: obsracle avoidance mode; 3: tracking

int g_modeComunication = 0; // 0:Infrared remote control 1:Bluetooth remote control

int g_AllState = 0; // 0: Busying; 1:Mode selection

//int g_IRRealse = 0; //Remote control buttons loosen detection

/Format string initialization/

int serial_putc( char c, struct __file * )

{

Serial.write( c );

return c;

}

void printf_begin(void)

{

fdevopen( &serial_putc, 0 );

}

void setup()

{

//Initialize motor drive for output mode

pinMode(Left_motor_go, OUTPUT);

pinMode(Left_motor_back, OUTPUT);

pinMode(Right_motor_go, OUTPUT);

pinMode(Right_motor_back, OUTPUT);

pinMode(Right_motor_en, OUTPUT);

pinMode(Left_motor_en, OUTPUT);

pinMode(BUZZER, OUTPUT);// Set buzzer as output

pinMode(left_led, OUTPUT);//Set led as output

pinMode(right_led, OUTPUT);//Set led as output

pinMode(KEY, INPUT_PULLUP);// Set button as input and internal pull-up mode

pinMode(Echo, INPUT); // Set Ultrasonic echo port as input

pinMode(Trig, OUTPUT); // Set Ultrasonic trig port as input

pinMode(SensorRight, INPUT); // Set Right Line Walking Infrared sensor as input

pinMode(SensorLeft, INPUT); // Set left Line Walking Infrared sensor as input

Serial.begin(9600); // Set Bluetooth baud rate 9600

digitalWrite(BUZZER, LOW); //Set beep mute

digitalWrite(Left_motor_en, HIGH); // set left motor enble

digitalWrite(Right_motor_en, HIGH); // set right motor enble

//Initialize state

g_carstate = enSTOP; // stop

g_modeComunication = 0; // Infrared Remote Control

g_modeSelect = 0; // remote mode

//Initialize Infrared decode

irrecv.enableIRIn();

pinMode(RECV_PIN, INPUT_PULLUP);

printf_begin();

}

void Distance_test() // Measuring front distance

{

digitalWrite(Trig, LOW); // set trig port low level for 2μs

delayMicroseconds(2);

digitalWrite(Trig, HIGH); // set trig port high level for 10μs(at least 10μs)

delayMicroseconds(10);

digitalWrite(Trig, LOW); // set trig port low level

float Fdistance = pulseIn(Echo, HIGH); // Read echo port high level time(unit:μs)

Fdistance = Fdistance / 58; // Distance(m) =(time(s) * 344(m/s)) / 2 /****** The speed of sound is 344m/s.*******/

// ==> 2*Distance(cm) = time(μs) * 0.0344(cm/μs)

// ==> Distance(cm) = time(μs) * 0.0172 = time(μs) / 58

Distance = Fdistance;

}

void run1() // Advance

{

digitalWrite(Left_motor_en,HIGH); // Left motor enable

analogWrite(Left_motor_en,157);

digitalWrite(Right_motor_en,HIGH); // Right motor enable

digitalWrite(Right_motor_go,HIGH); // right motor go ahead

digitalWrite(Right_motor_back,LOW);

analogWrite(Right_motor_go,210);//PWM–Pulse Width Modulation(0~255). right motor go speed is 255.

analogWrite(Right_motor_back,0);

digitalWrite(Left_motor_go,HIGH); // set left motor go ahead

digitalWrite(Left_motor_back,LOW);

analogWrite(Left_motor_go,130);//PWM–Pulse Width Modulation(0~255).left motor go speed is 135.

analogWrite(Left_motor_back,0);

digitalWrite(left_led, LOW);

digitalWrite(right_led, LOW);

//delay(time * 100); //Running time can be adjusted

}

void brake() //Stop

{

digitalWrite(Left_motor_back, LOW);

digitalWrite(Left_motor_go, LOW);

digitalWrite(Right_motor_go, LOW);

digitalWrite(Right_motor_back, LOW);

digitalWrite(left_led, HIGH);

digitalWrite(right_led, HIGH);

}

void left() //Turn left

{

digitalWrite(Right_motor_go,HIGH); // right motor go ahead

digitalWrite(Right_motor_back,LOW);

analogWrite(Right_motor_go,250); // PWM–Pulse Width Modulation(0~255) control speed,right motor go speed is 255.

analogWrite(Right_motor_back,0);

digitalWrite(Left_motor_go,LOW); // left motor stop

digitalWrite(Left_motor_back,LOW);

analogWrite(Left_motor_go,0);

analogWrite(Left_motor_back,0);

digitalWrite(left_led, HIGH);

digitalWrite(right_led, LOW);

}

void spin_left() //Left rotation

{

digitalWrite(Right_motor_go,HIGH);// right motor go ahead

digitalWrite(Right_motor_back,LOW);

analogWrite(Right_motor_go,200);// PWM–Pulse Width Modulation(0~255) control speed ,right motor go speed is 200.

analogWrite(Right_motor_back,0);

digitalWrite(Left_motor_go,LOW); // left motor back off

digitalWrite(Left_motor_back,HIGH);

analogWrite(Left_motor_go,0);

analogWrite(Left_motor_back,200);// PWM–Pulse Width Modulation(0~255) control speed,left motor back speed is 200.

digitalWrite(left_led, HIGH);

digitalWrite(right_led, LOW);

}

void right() //turn right

{

digitalWrite(Right_motor_go,LOW); // right motor stop

digitalWrite(Right_motor_back,LOW);

analogWrite(Right_motor_go,0);

analogWrite(Right_motor_back,0);

digitalWrite(Left_motor_go,HIGH);// left motor go ahead

digitalWrite(Left_motor_back,LOW);

analogWrite(Left_motor_go,230);// PWM–Pulse Width Modulation(0~255) control speed ,left motor go speed is 255.

analogWrite(Left_motor_back,0);

digitalWrite(left_led, LOW);

digitalWrite(right_led, HIGH);

}

void spin_right() //Right rotation

{

digitalWrite(Right_motor_go,LOW); // right motor back off

digitalWrite(Right_motor_back,HIGH);

analogWrite(Right_motor_go,0);

analogWrite(Right_motor_back,200);// PWM–Pulse Width Modulation(0~255) control speed

digitalWrite(Left_motor_go,HIGH);// left motor go ahead

digitalWrite(Left_motor_back,LOW);

analogWrite(Left_motor_go,200);// PWM–Pulse Width Modulation(0~255) control speed

analogWrite(Left_motor_back,0);

digitalWrite(left_led, LOW);

digitalWrite(right_led, HIGH);

}

void back() //back off

{

digitalWrite(Right_motor_go,LOW); //right motor back off

digitalWrite(Right_motor_back,HIGH);

analogWrite(Right_motor_go,0);

analogWrite(Right_motor_back,150);// PWM–Pulse Width Modulation(0~255) control speed

analogWrite(Right_motor_en,165);

digitalWrite(Left_motor_go,LOW); //left motor back off

digitalWrite(Left_motor_back,HIGH);

analogWrite(Left_motor_go,0);

analogWrite(Left_motor_back,140);// PWM–Pulse Width Modulation(0~255) control speed

digitalWrite(left_led, LOW);

digitalWrite(right_led, HIGH);

//led();

}

void whistle() //beep sounds

{

/* int i;

for (i = 0; i < 15; i++) //Output one frequency sound

{

digitalWrite(BUZZER, LOW); //sounds

delay(10);// delay 10ms

digitalWrite(BUZZER, HIGH); //mute

delay(1);// delay 1ms

}*/

digitalWrite(BUZZER, HIGH); //sounds

delay(2000);//delay 2s

digitalWrite(BUZZER, LOW); //mute

// delay(2);//delay 2s

//}

}

/Bluetooth receive/

void Bluetooth(void)

{

if (newLineReceived)

{

//Determine if mode selection or not

if (inputString[1] == ‘M’ && inputString[2] == ‘O’ && inputString[3] == ‘D’ && inputString[4] == ‘E’)

{

if (inputString[6] == ‘0’) //stop

{

g_carstate = enSTOP;

g_modeSelect = 0;

g_AllState = 0;

BeepOnOffMode();

}

else

{

switch (inputString[5])//the fifth bit in the string (0:remote control mode(default); 1:line walking mode ; 2: obsracle avoidance mode; 3: tracking)

{

case ‘0’: g_modeSelect = 0; break;

case ‘1’: g_modeSelect = 1; break;

case ‘2’: g_modeSelect = 2; break;

case ‘3’: g_modeSelect = 3; break;

default: g_modeSelect = 0; break;

}

g_AllState = 0;

BeepOnOffMode();

}

}

else if (g_modeSelect == 0 && g_AllState == 0) //remote control mode(default)

{

switch (inputString[1]) //Direction

{

case run_car: g_carstate = enRUN; break;

case back_car: g_carstate = enBACK; break;

case left_car: g_carstate = enLEFT; break;

case right_car: g_carstate = enRIGHT; break;

case stop_car: g_carstate = enSTOP; break;

default: g_carstate = enSTOP; break;

}

if (inputString[3] == ‘1’) //Left rotation

{

spin_left();

delay(2000);//delay 2s

brake();

}

else if (inputString[3] == ‘2’) //Right rotation

{

spin_right();

delay(2000);

brake();

}

if (inputString[5] == ‘1’) //beep sounds

{

whistle();

}

if (inputString[7] == ‘1’) //speed up

{

control += 50;

if (control > 255)

{

control = 255;

}

}

if (inputString[9] == ‘1’) //speed reduction

{

control -= 50;

if (control < 50)

{

control = 100;

}

}

}

inputString = “”; // clear the string

newLineReceived = false;

}

}

void Key_Scan(void)

{

int val;

while (!digitalRead(KEY)) // When the button is pressed

{

delay(10);

val = digitalRead(KEY);// Reads the button ,the level value assigns to val

if (val == LOW) //Double check the button is pressed

{

if (g_modeComunication == 0)// In Infrared remote control

{

g_modeComunication = 1; // Switch to Bluetooth remote control

//digitalWrite(LED, HIGH); //led lights up

}

else//In Bluetooth remote control

{

g_modeComunication = 0; //Switch to Infrared remote control

//digitalWrite(LED, LOW); led lights off

}

digitalWrite(BUZZER, HIGH); //beep sounds

delay(100);//100ms

digitalWrite(BUZZER, LOW); //beep mute

while (!digitalRead(KEY)); //Determine if the button is released or not

}

else

digitalWrite(BUZZER, LOW); //beep mute

}

}

//Car running control

void CarControl()

{

if (g_modeSelect != 2 )

{

switch (g_carstate)

{

case enSTOP: brake(); break;

case enRUN: run1(); break;

case enLEFT: left(); break;

case enRIGHT: right(); break;

case enBACK: back(); break;

case enTLEFT: spin_left(); break;

case enTRIGHT: spin_right(); break;

default: brake(); break;

}

}

}

void IR_Deal()

{

if (irrecv.decode(&results)) //Infrared received result

{

//Serial.println(results.value, HEX);

//if (((results.value >> 16) & 0x0000ffff) == 0x00ff)

//{

//printf(“$AR,HSX,%08lX#\n”, results.value);

//According to the different values to perform different operations

// 00FD10EF 7 mode off

// 00FDA05F 5 NC

// 00FD609F 6 NC

// 00FD50AF 9 mode play

// 00FD906F 8 NC

// 00FDB04F 0 beep

// 00FD8877 up Advance

// 00FD28D7 < Turn left

// 00FDA857 ok Stop

// 00FD6897 > Turn right

// 00FD9867 DW Back

// 00FD30CF * Left rotation

// 00FD708F # right rotation

// 00FD00FF 1 remote control mode 1

// 00FD807F 2 obstacle avoidance mode 2

// 00FD40BF 3 line walking mode 3

// 00FD20DF 4 tacking mode 4

switch (results.value)

{

case 0x00FD10EF: g_carstate = enSTOP; g_AllState = 0; g_modeSelect = 0; BeepOnOffMode() ;break; // 7 mode off

case 0x00FD50AF: g_carstate = enSTOP; g_AllState = 0; BeepOnOffMode() ; break; // 9 mode play

//case 0x00FFE01F: g_AllState = 1; g_modeSelect–; if (g_modeSelect == -1) g_modeSelect = 3; break;

//case 0x00FF906F: g_AllState = 1; g_modeSelect++; if (g_modeSelect == 4) g_modeSelect = 0; break;

case 0x00FD00FF: g_AllState = 1; g_modeSelect = 0; ModeBEEP(g_modeSelect); break; // 1 remote control mode 1

case 0x00FD807F: g_AllState = 1; g_modeSelect = 2; ModeBEEP(g_modeSelect); break; // 2 obstacle avoidance mode 2

case 0x00FD40BF: g_AllState = 1; g_modeSelect = 1; ModeBEEP(g_modeSelect); break; //3 line walking mode 3

case 0x00FD20DF: g_AllState = 1; g_modeSelect = 3; ModeBEEP(g_modeSelect); break; //4 tacking mode 4

default: break;

}

if (g_modeSelect == 0 && g_AllState == 0)

{

switch (results.value)

{

//case 0x00FF02FD: control += 50; if (control > 255) control = 255; break;

//case 0x00FF9867: control -= 50; if (control < 50) control = 100; break;

case 0x00FDB04F: whistle(); break; // 0 beep OFF/ON

case 0x00FD8877: g_carstate = enRUN; break; // up Advance

case 0x00FD28D7: g_carstate = enLEFT; break; // < Turn left

case 0x00FDA857: g_carstate = enSTOP; break; // ok Stop

case 0x00FD6897: g_carstate = enRIGHT; break; // > Turn right

case 0x00FD9867: g_carstate = enBACK; break; // DW Back

case 0x00FD30CF: g_carstate = enTLEFT; break; // * Left rotation

case 0x00FD708F: g_carstate = enTRIGHT; break; // # right rotation

default: break; //Stay the same

}

}

//}

last = millis();

irrecv.resume(); // received next Infrared decode

}

else if (millis() - last > 120)

{

g_carstate = enSTOP;

last = millis();

}

}

//mode display

void ModeBEEP(int mode)

{

for (int i = 0; i < mode + 1; i++)

{

digitalWrite(BUZZER, HIGH); //beep sounding

delay(100);

digitalWrite(BUZZER, LOW); //mute

delay(100);

}

delay(100);

digitalWrite(BUZZER, LOW); //mute

}

//buzzer sounds for 1s to wait mode selection

void BeepOnOffMode()

{

digitalWrite(BUZZER, HIGH); //beep sounding

delay(1000);

digitalWrite(BUZZER, LOW); //mute

}

//line walking mode

void track()

{

/**************************************************************************************

Infrared signal back means white undersurface ,returns low level and led lights up.

Infrared signal gone means black undersurface ,returns high level and led lights off.

**************************************************************************************/

SR = digitalRead(SensorRight);//Right Line Walking Infrared sensor against white undersurface,then LED[L2] light illuminates and while against black undersurface,LED[L2] goes off

SL = digitalRead(SensorLeft);//Left Line Walking Infrared sensor against white undersurface,then LED[L3] light illuminates and while against black undersurface,LED[L3] goes off

if (SL == LOW && SR == LOW) // Black lines were not detected at the same time

g_carstate = enRUN; // go ahead

else if (SL == LOW & SR == HIGH)// Left sensor against white undersurface and right against black undersurface , the car left off track and need to adjust to the right.

g_carstate = enRIGHT;

else if (SR == LOW & SL == HIGH) // Rihgt sensor against white undersurface and left against black undersurface , the car right off track and need to adjust to the left.

g_carstate = enLEFT;

else // Black lines were detected at the same time , the car stop.

g_carstate = enSTOP;

}

// ultrason_obstacle_avoid

void ultrason_obstacle_avoiding()

{

Distance_test();// Measuring front distance

if (Distance < 38) ////The value is the distance that meets the obstacle, and can be set according to the actual situation

{

delay(10);

Distance_test();////Measuring front distance

while (Distance < 38) //Determine whether there is an obstruction again.If there is obstacle , turn the direction and determine again

{

spin_right();//Right rotation for 400ms

delay(400);

brake();//stop

Distance_test();////Measuring front distance

}

}

else

run1();//There is nothing obstacled. Go Advance

}

// infrared follow mode

void Infrared_follow()

{

/**************************************************************************************

Infrared signal back means there is something obstacled ,returns low level and led lights up.

Infrared signal gone means there is nothing obstacled ,returns high level and led lights off.

**************************************************************************************/

SR_2 = digitalRead(SensorRight_2);//Right infrared sensor detects the obstacle,then LED[L5] light illuminates and otherwise it goes off.

SL_2 = digitalRead(SensorLeft_2);//Left infrared sensor detects the obstacle,then LED[L4] light illuminates and otherwise it goes off.

if (SL_2 == LOW && SR_2 == LOW)//There is something obstacled ,goes and follow it.

g_carstate = enRUN;

else if (SL_2 == HIGH & SR_2 == LOW)// There is something obstacled on the right then LED[L4] light illuminates,turns right and follow.

g_carstate = enRIGHT;

else if (SR_2 == HIGH & SL_2 == LOW)// There is something obstacled on the left then LED[L4] light illuminates,turns left and follow.

g_carstate = enLEFT;

else // There is nothing obstacled , stop.

g_carstate = enSTOP;

}

/main loop/

void loop()

{

/Check button press/

Key_Scan();

if (g_modeComunication == 0) //Infrared Remote Control mode

{

IR_Deal();

}

else//Bluetooth Remote Control mode

{

Bluetooth();

}

// Switch different mode

if (g_AllState == 0)

{

switch (g_modeSelect)

{

case 1: track(); break; // Line walking mode

case 2: ultrason_obstacle_avoiding(); break;// Obstacle avoidance mode

case 3: Infrared_follow(); break;// Tracking mode

}

}

CarControl();

}

//Serial read data

void serialEvent()

{

while (Serial.available())

{

incomingByte = Serial.read(); //One byte by one byte reads

if (incomingByte == ‘$’) // ‘$’ means the start of packet

{

startBit = true;

}

if (startBit == true)

{

inputString += (char) incomingByte; // The received data constitutes a completed packet.

}

if (incomingByte == ‘#’) // ‘#’ means the end of packet

{

newLineReceived = true;

startBit = false;

}

}

}

After this im not able to get the result from the robot :frowning: :frowning: :frowning:

How about adding code tags around your code?

Exactly what doesn’t work?

You might find someone who’s willing to sift through your code trying to find something somewhere that’s not quite right, but you also might not.