Here are some questions and such that are very open for discussion. I am interested in most of the COG boards for one reason or another.
-
WHY is there a MALE DB9 on the Breakout COG? This seems like it serves only to make connection to it more difficult than if it had a FEMALE DB9.
-
Will there be an FPGA/ARM7 COG available sometime soon?
It would be great to see a medium to large FPGA such as the Xilinx Spartan 3E 1600 gate or similar Altera FPGA coupled with some onboard intelligence like an LPC-2148 or maybe an LPC2294 or even the massive LPC-2378. More processing power and I/O is always better!
A COG like this could also standalone for many uses, and be able to be an I2C/SPI Master OR Slave and still be able to communicate with other I2C/SPI devices and subsystems, since the MCU would have two I2C and two SPI interfaces. I see the FPGA as being accessible from the outside and/or by the onboard MCU.
-
Are there any plans to make an 1.MX27 or i.MX31 COG? I’m really more interested in the i.MX27 (404 BGA) than the i.MX21. The i.MX31 is a 457 BGA.
-
Regarding the Robotics COG, I think the H-Bridges are a little low on power. They should be at least 5A each for up to 12V or 24V motors. The onboard MCU should be at least an LPC-2148. This would allow it to be an I2C/SPI SLAVE to the i.MX21 COG as well as still be an I2C/SPI Master (or any combination) to communicate with other I2C/SPI sensors and subsystems. This would make it much more useful in standalone mode also.
I can see a full blown COG stack being mounted on my power wheelchair, including the Multi-Media COG with a full touchscreen interface. This would make an excellent onboard computer/controller, especially with the addition of a WiFi/GPS COG.
I’m probably just dreaming of these things, but they would sure be AWESOME to have.
If I am going to dream, I might as well dream BIG! ![]()
8-Dale