Transmission format JSON
Currently transmission protocol MQTT
this
Currently, I would like to replace it with the transmission protocol AMQT or HTTP protocol.
What should I do for this?
please tell me.
Hope is Arduino.
If it is not possible, you can use other software.
However, it is necessary to be able to write software only serially like Arduino.
Program example (This program is operating normally after confirming transmission and reception on WINDOWS AZURE)
#include <stdio.h>
#include <String.h>
#include <WiFi.h>
#include “Esp32MQTTClient.h”
loop ()
{
“Omitted”
Char A [150]
snprintf (A, 150, "{" NO1 \ ": " 202009 \ ", " NO2 \ ":% 4d, " NO3 \ ":% 4d, ":% 4d, \ "NO4 ": \ "NG "} ", tempreature, sumtime, flow, pressure, Status_);
if (Esp32MQTTClient_SendEvent (& A [0])) {}
“Omitted”
}
====================