Hello,
I am getting a lot of compiler errors. I think there is a mismatch between support libraries and naming conventions used in the main code. Does anyone have updated code that will run on a Sparkfun redone plus board with weather shield? I am running IDE 2.3.4
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino:75:1: error: ‘Weather’ does not name a type
Weather myHumidity; //Create an instance of the humidity sensor
^~~~~~~
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino: In function ‘void setup()’:
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino:99:3: error: ‘myHumidity’ was not declared in this scope
myHumidity.begin();
^~~~~~~~~~
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino:99:3: note: suggested alternative: ‘humidity’
myHumidity.begin();
^~~~~~~~~~
humidity
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino: In function ‘void calcWeather()’:
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino:140:14: error: ‘myHumidity’ was not declared in this scope
humidity = myHumidity.getRH();
^~~~~~~~~~
C:\Users\nicka\OneDrive\Documents\Arduino\Sparkfun_Weather_Station\Sparkfun_Weather_Station.ino:140:14: note: suggested alternative: ‘humidity’
humidity = myHumidity.getRH();
^~~~~~~~~~
humidity
exit status 1
Compilation error: ‘Weather’ does not name a type
/*
Weather Shield Example
By: Nathan Seidle
SparkFun Electronics
Date: November 16th, 2013
License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).
Much of this is based on Mike Grusin's USB Weather Board code: https://www.sparkfun.com/products/10586
This is a more advanced example of how to utilize every aspect of the weather shield. See the basic
example if you're just getting started.
This code reads all the various sensors (wind speed, direction, rain gauge, humidity, pressure, light, batt_lvl)
and reports it over the serial comm port. This can be easily routed to a datalogger (such as OpenLog) or
a wireless transmitter (such as Electric Imp).
Measurements are reported once a second but windspeed and rain gauge are tied to interrupts that are
calculated at each report.
This example code assumes the GPS module is not used.
Updated by Joel Bartlett
03/02/2017
Removed HTU21D code and replaced with Si7021
Updated be Wes Furuya
06/19/2023
Implemented "Weather Meter" Arduino library
*/
#include <Wire.h> //I2C needed for sensors
#include "SparkFunMPL3115A2.h" //Pressure sensor - Search "SparkFun MPL3115" and install from Library Manager
#include "SparkFun_Si7021_Breakout_Library.h" //Humidity sensor - Search "SparkFun Si7021" and install from Library Manager
#include "SparkFun_Weather_Meter_Kit_Arduino_Library.h" //Weather meter kit - Search "SparkFun Weather Meter" and install from Library Manager
//Hardware pin definitions
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
// digital I/O pins
const byte WSPEED = 3;
const byte RAIN = 2;
const byte STAT1 = 7;
const byte STAT2 = 8;
// analog I/O pins
const byte REFERENCE_3V3 = A3;
const byte LIGHT = A1;
const byte BATT = A2;
const byte WDIR = A0;
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
//Global Variables
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
long lastSecond; //The millis counter to see when a second rolls by
float humidity = 0; // [%]
float tempf = 0; // [temperature F]
//float baromin = 30.03;// [barom in] - It's hard to calculate baromin locally, do this in the agent
float pressure = 0;
float wind_dir = 0; // [degrees (Cardinal)]
float wind_speed = 0; // [kph]
float rain = 0; // [mm]
float batt_lvl = 11.8; //[analog value from 0 to 1023]
float light_lvl = 455; //[analog value from 0 to 1023]
//-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=-=
MPL3115A2 myPressure; //Create an instance of the pressure sensor
Weather myHumidity; //Create an instance of the humidity sensor
SFEWeatherMeterKit myweatherMeterKit(WDIR, WSPEED, RAIN); // Create an instance of the weather meter kit
void setup() {
Serial.begin(115200);
Serial.println("Weather Shield Example");
pinMode(STAT1, OUTPUT); //Status LED Blue
pinMode(STAT2, OUTPUT); //Status LED Green
// pinMode(WSPEED, INPUT_PULLUP); // input from wind meters windspeed sensor
// pinMode(RAIN, INPUT_PULLUP); // input from wind meters rain gauge sensor
pinMode(REFERENCE_3V3, INPUT);
pinMode(LIGHT, INPUT);
//Configure the pressure sensor
myPressure.begin(); // Get sensor online
myPressure.setModeBarometer(); // Measure pressure in Pascals from 20 to 110 kPa
myPressure.setOversampleRate(7); // Set Oversample to the recommended 128
myPressure.enableEventFlags(); // Enable all three pressure and temp event flags
//Configure the humidity sensor
myHumidity.begin();
// The weather meter kit library assumes a 12-bit ADC
// Configuring a 10-bit ADC resolution for the ATmega328 (RedBoard/Uno)
myweatherMeterKit.setADCResolutionBits(10);
// Begin weather meter kit
myweatherMeterKit.begin();
lastSecond = millis();
// // attach external interrupt pins to IRQ functions
// attachInterrupt(0, rainIRQ, FALLING);
// attachInterrupt(1, wspeedIRQ, FALLING);
// // turn on interrupts
// interrupts();
Serial.println("Weather Shield online!");
}
void loop() {
//Keep track of which minute it is
if (millis() - lastSecond >= 1000) {
digitalWrite(STAT1, HIGH); //Blink stat LED
lastSecond += 1000;
//Report all readings every second
printWeather();
}
digitalWrite(STAT1, LOW); //Turn off stat LED
delay(100);
}
//Calculates each of the variables that wunderground is expecting
void calcWeather() {
//Calc temp/humidity from Si7021 sensor
humidity = myHumidity.getRH();
tempf = myHumidity.readTempF();
//Weather Meter Kit
//Calc Wind
wind_dir = myweatherMeterKit.getWindDirection();
wind_speed = myweatherMeterKit.getWindSpeed();
//Calc Rain
rain = myweatherMeterKit.getTotalRainfall();
//Calc pressure from MPL3115A2
pressure = myPressure.readPressure();
//Calc light level
light_lvl = get_light_level();
//Calc battery level
batt_lvl = get_battery_level();
}
//Returns the voltage of the light sensor based on the 3.3V rail
//This allows us to ignore what VCC might be (an Arduino plugged into USB has VCC of 4.5 to 5.2V)
float get_light_level() {
float operatingVoltage = analogRead(REFERENCE_3V3);
float lightSensor = analogRead(LIGHT);
operatingVoltage = 3.3 / operatingVoltage; //The reference voltage is 3.3V
lightSensor = operatingVoltage * lightSensor;
return (lightSensor);
}
//Returns the voltage of the raw pin based on the 3.3V rail
//This allows us to ignore what VCC might be (an Arduino plugged into USB has VCC of 4.5 to 5.2V)
//Battery level is connected to the RAW pin on Arduino and is fed through two 5% resistors:
//3.9K on the high side (R1), and 1K on the low side (R2)
float get_battery_level() {
float operatingVoltage = analogRead(REFERENCE_3V3);
float rawVoltage = analogRead(BATT);
operatingVoltage = 3.30 / operatingVoltage; //The reference voltage is 3.3V
rawVoltage = operatingVoltage * rawVoltage; //Convert the 0 to 1023 int to actual voltage on BATT pin
rawVoltage *= 4.90; //(3.9k+1k)/1k - multiple BATT voltage by the voltage divider to get actual system voltage
return (rawVoltage);
}
//Prints the various variables directly to the port
//I don't like the way this function is written but Arduino doesn't support floats under sprintf
void printWeather() {
calcWeather(); //Go calc all the various sensors
Serial.println();
Serial.print("humidity=");
Serial.print(humidity, 1);
Serial.print(" %RH, tempf=");
Serial.print(tempf, 1);
Serial.print(" F, pressure=");
Serial.print(pressure, 2);
Serial.print(" Pa, wind direction= ");
Serial.print(wind_dir, 1);
Serial.print(" deg, wind speed= ");
Serial.print(wind_speed, 1);
Serial.print(" kph, total rain= ");
Serial.print(rain, 1);
Serial.print(" mm, batt_lvl=");
Serial.print(batt_lvl, 2);
Serial.print(" V, light_lvl=");
Serial.print(light_lvl, 2);
Serial.print(",");
Serial.println("#");
}