Hi again,
I got the watch and sold it, inserted the battery and it seems to work.
I tried to connect the programmer in order to change the code to 24 hours instead of 12 hours as initial test.
It doesn’t work (and now the watch doesn’t work either), I’m missing something.
I need assistance in order to solve this.
BTW, can flipping the programmer pins damage the board?
I have sold the programmer pins in order to ensure a good connection.
The attached pictures show the connection and the software configuration.
I get the following error:
Arduino: 1.8.13 (Windows 10), Board: "Arduino Pro or Pro Mini, ATmega328P (3.3V, 8 MHz)"
C:\Program Files (x86)\Arduino\arduino-builder -dump-prefs -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Otaku\Documents\Arduino\libraries -fqbn=arduino:avr:pro:cpu=8MHzatmega328 -vid-pid=0403_6001 -ide-version=10813 -build-path C:\Users\Otaku\AppData\Local\Temp\arduino_build_410569 -warnings=none -build-cache C:\Users\Otaku\AppData\Local\Temp\arduino_cache_633412 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arduinoOTA.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.arduinoOTA-1.3.0.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude-6.3.0-arduino17.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc-7.3.0-atmel3.6.1-arduino7.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -verbose D:\My Documents\Desktop\bigwatch\BigTime\BigTime.ino
C:\Program Files (x86)\Arduino\arduino-builder -compile -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\Otaku\Documents\Arduino\libraries -fqbn=arduino:avr:pro:cpu=8MHzatmega328 -vid-pid=0403_6001 -ide-version=10813 -build-path C:\Users\Otaku\AppData\Local\Temp\arduino_build_410569 -warnings=none -build-cache C:\Users\Otaku\AppData\Local\Temp\arduino_cache_633412 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arduinoOTA.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.arduinoOTA-1.3.0.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avrdude-6.3.0-arduino17.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -prefs=runtime.tools.avr-gcc-7.3.0-atmel3.6.1-arduino7.path=C:\Program Files (x86)\Arduino\hardware\tools\avr -verbose D:\My Documents\Desktop\bigwatch\BigTime\BigTime.ino
Using board 'pro' from platform in folder: C:\Program Files (x86)\Arduino\hardware\arduino\avr
Using core 'arduino' from platform in folder: C:\Program Files (x86)\Arduino\hardware\arduino\avr
Detecting libraries used...
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-g++" -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=8000000L -DARDUINO=10813 -DARDUINO_AVR_PRO -DARDUINO_ARCH_AVR "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\cores\\arduino" "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\variants\\eightanaloginputs" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\sketch\\BigTime.ino.cpp" -o nul -DARDUINO_LIB_DISCOVERY_PHASE
Generating function prototypes...
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-g++" -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -flto -w -x c++ -E -CC -mmcu=atmega328p -DF_CPU=8000000L -DARDUINO=10813 -DARDUINO_AVR_PRO -DARDUINO_ARCH_AVR "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\cores\\arduino" "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\variants\\eightanaloginputs" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\sketch\\BigTime.ino.cpp" -o "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\preproc\\ctags_target_for_gcc_minus_e.cpp" -DARDUINO_LIB_DISCOVERY_PHASE
"C:\\Program Files (x86)\\Arduino\\tools-builder\\ctags\\5.8-arduino11/ctags" -u --language-force=c++ -f - --c++-kinds=svpf --fields=KSTtzns --line-directives "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\preproc\\ctags_target_for_gcc_minus_e.cpp"
Compiling sketch...
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-g++" -c -g -Os -w -std=gnu++11 -fpermissive -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics -Wno-error=narrowing -MMD -flto -mmcu=atmega328p -DF_CPU=8000000L -DARDUINO=10813 -DARDUINO_AVR_PRO -DARDUINO_ARCH_AVR "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\cores\\arduino" "-IC:\\Program Files (x86)\\Arduino\\hardware\\arduino\\avr\\variants\\eightanaloginputs" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\sketch\\BigTime.ino.cpp" -o "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\sketch\\BigTime.ino.cpp.o"
Compiling libraries...
Compiling core...
Using precompiled core: C:\Users\Otaku\AppData\Local\Temp\arduino_cache_633412\core\core_arduino_avr_pro_cpu_8MHzatmega328_0c812875ac70eb4a9b385d8fb077f54c.a
Linking everything together...
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-gcc" -w -Os -g -flto -fuse-linker-plugin -Wl,--gc-sections -mmcu=atmega328p -o "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.elf" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569\\sketch\\BigTime.ino.cpp.o" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/..\\arduino_cache_633412\\core\\core_arduino_avr_pro_cpu_8MHzatmega328_0c812875ac70eb4a9b385d8fb077f54c.a" "-LC:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569" -lm
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-objcopy" -O ihex -j .eeprom --set-section-flags=.eeprom=alloc,load --no-change-warnings --change-section-lma .eeprom=0 "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.elf" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.eep"
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-objcopy" -O ihex -R .eeprom "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.elf" "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.hex"
"C:\\Program Files (x86)\\Arduino\\hardware\\tools\\avr/bin/avr-size" -A "C:\\Users\\Otaku\\AppData\\Local\\Temp\\arduino_build_410569/BigTime.ino.elf"
Sketch uses 4390 bytes (14%) of program storage space. Maximum is 30720 bytes.
Global variables use 222 bytes (10%) of dynamic memory, leaving 1826 bytes for local variables. Maximum is 2048 bytes.
C:\Program Files (x86)\Arduino\hardware\tools\avr/bin/avrdude -CC:\Program Files (x86)\Arduino\hardware\tools\avr/etc/avrdude.conf -v -patmega328p -carduino -PCOM5 -b57600 -D -Uflash:w:C:\Users\Otaku\AppData\Local\Temp\arduino_build_410569/BigTime.ino.hex:i
avrdude: Version 6.3-20190619
Copyright (c) 2000-2005 Brian Dean, [http://www.bdmicro.com/](http://www.bdmicro.com/)
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "C:\Program Files (x86)\Arduino\hardware\tools\avr/etc/avrdude.conf"
Using Port : COM5
Using Programmer : arduino
Overriding Baud Rate : 57600
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 1 of 10: not in sync: resp=0xe0
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 2 of 10: not in sync: resp=0xe0
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 3 of 10: not in sync: resp=0xe0
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 4 of 10: not in sync: resp=0xe0
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 5 of 10: not in sync: resp=0xe0
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 6 of 10: not in sync: resp=0xe0
avrdude: stk500_getsync() attempt 7 of 10: not in sync: resp=0x00
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 8 of 10: not in sync: resp=0x00
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 9 of 10: not in sync: resp=0x00
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 10 of 10: not in sync: resp=0x00
avrdude done. Thank you.
Problem uploading to board. See [http://www.arduino.cc/en/Guide/Troubleshooting#upload](http://www.arduino.cc/en/Guide/Troubleshooting#upload) for suggestions.
I thought the problem was with the baud rate and tried to run it from a command window without -b57600, but it didn’t help.
Links to the pictures (for some reason I can’t attach them on the form)
https://ibb.co/Ryb0R3j
https://ibb.co/cYKjB90