connecting RF module to breadboard

i’d like to order an RF module (link below), but it doesn’t come in DIP packaging or have hole pins which can be used with headers to connect to a breadboard… is there any sort of adapter that can take these types of pins and allow me to connect it to a breadboard?

picture here:

http://www.amber-wireless.de/en/produkt … 7388526475

thanks!

You’ll need to get a PCB made.

Leon

Those side-facet pads look pretty big, and sorta like they’re 0.1in. You might be able to solder pin headers right to em, and then put that directly into a protoboard. Then put pin headers into the protoboard to go to your breadboard. [The reason for the two step process is that those little pads don’t look like they could take much torque].

Cheers,

–David Carne

I have some “mainboards” for board with these SMT pads. The mainboards have V-shaped spring-wire connectors so you can insert/remove the module. Intended for prototypes, not sturdy enough for field use.

Here’s an example

http://www.helicomm.com/showproducts.asp?ID=132

This mainboard (motherboard) uses that company’s 802.15.4 modules which have that SMT style connector.

I suppose you can dig and dig and find out what vendor makes those spring connectors.