Its a great screen, but the connector was SMD and the pins are too small for a human to attempt to solder them so I was hoping to see if anyone knows of a connector or breakout I can plug this into for reuse.
I looked around here but all the breakouts already have screens attached. Am I doomed?
Unfortunately, you might be! We spend quite some time finding appropriate connectors for ribbon cables such as that. There may be a connector, but it’s probably SMD! Is there a connector on the board that you can hot-air off?
I have 4 of these screens, looking for a socket. Tried removing the little bugger but its so tiny no hope. I work in I.T. and we have a box full of old damaged, out of waranty blackberry’s and I have removed the screens. I would love to use then in my project.
That looks like a good candidate for coaxing off with a hot-air tool to me.
Alternately, it might even work with the “giant-blob-of-molten-solder-covering-all-the-pins-on-one-side-so-you-can-lift-one-side-at-a-time” desoldering approach.
I have one too, also from a Blackberry, and I managed to take out the connector. Originally, I wanted to use it with a microcontroller (I don’t expect it to be easy). But after googling for an hour, I couldn’t find any datasheet or application information, only selling leads. Does anyone has a datasheet for this device ?
And on it’s back there are 2 labels saying: ACX346AKN-8 726A43F and LCD-08818 001/003.
The on-board controller is a flip-chip, with nothing written on it, but on the flexible band says: LMF-083. Googled for this one too, but nothing usefull. Are there equivalent displays to this one ? Are the pins standardized so i can find them in other displays ( similar to the lcd modules with HD44780) ?