Hello Forum,
I have three sets of two LEDEngin LZ1’s: two LZ1-00UV0R, which typically run at 3.5V, 700mA; two LZ1-00DB00, which typically run at 3.2 V, 1000mA and two LZ1-00CW02, which typically run at 2.8V, 1000mA. I would like to be able to separately control each set of two with an Arduino. Are there similar projects that anyone might be able to point me to?
thanks