Im using the TI Code Composer suite with an ARM 7 and Im looking for a way to get the CPSR back into a C variable. I was looking through the documentation that came with the compiler and it didnt have quite what I was looking for. What Im looking for is the state of the interrupt disable bit. I need to use this bit as a condition variable for something like:
if (interrupts enabled){
do this
}
the inline asm syntax is just
asm("assembly");
The problem is, Im not sure how to associate some C variable to the asm code to pass the CPSR back to the C code flow. Ive used other compilers in the past that have an option to pass arguments to the asm code like
_asm("tfr b, ccr",foo);
which passes the condition code register (for an HC12) to the var foo, but this compiler does not have that capability. How would I do the above with this compiler?