Hello,
I’m a new user of the ADuC7026 board, and am playing with it using Rowley crossworks (I’m an MPLAB pup so I like the integrated development environments).
I have both a 20 pin olimex parallel port JTAG, and the USB tiny JTAG and have two questions:
- How do I go about loading to the flash of the micro? I can get it to go in the debug mode no problem, but when I tell it to build in ARM FLASH RELEASE and load the .elf file… the chip doesn’t run

When I do a ‘build and run’ in either ARM FLASH RELEASE or THUMB FLASH RELEASE, the chip runs until I reset it, making me question the nature of the flash loading ![]()
- Is it possible to use the Olimex USB tiny JTAG with crossworks?
Thanks in advance.