I’m trying to export a custom package from an existing board layout / schematic in EAGLE. It’s the package for the PixArt camera in the front of the WiiMote.
I found a layout using this sensor here:
http://www.cc-zwei.de/wiki/index.php/AT … _IR_Sensor
Where the download containing the eagle files can be found here:
http://www.cczwei.de/atm18_downloads/wi … sensor.zip
However, there was no library I could download. Only the schematics and the board layout – can I export the package from the existing files into a library? When I check the properties of the wii camera inside the EAGLE files I see the following (as attached).
Any help would be greatly appreciated!
![]()