Hi,
I am using 9 large (10 inches) seven segment display in my project which I am driving using ESP32.
Unfortunately I am having trouble with digit 7,8 & 9. The segments from these 3 digits which are supposed to be OFF aren’t completely off sometimes. When I have digit 1 - 6 displaying numbers which need lesser segments ON, digit 7-9 works fine (the segments which are meant to be OFF will be OFF). But when I, for example, display number 8 for digits 1-6, I see the problem with digits 7-9.
When I measure the voltage b/w the segment (& 12V pin)) when having trouble I see it ranging from 0v (when working correctly) to various voltages like ~3V, ~6V.
I don’t have electronics background and relying on online materials for my project.
Thanks in advance for your time
Cheers