People
I can compile my source without problems (using Yagarto), and start the debugger too, but something stranger was happening. I put breakpoints and nothing happens, and always that I pause it stops on undefined function. And I can’t see the pin toggle. But when I flash the device using the LPC flash tools, it works.
I follow all steps for installation of Yagarto … I’m trying debug the demo2106_flash from Mr Lynch, this debugger works only with ram one?
Other question:
When I try use the example code in RAM, with LPC Flash Utility I get this message: Code in HEX file exceeds Flash Limitations. But it compile OK.
Any help or suggestion will be very appreciated,
Thks,
Leonardo de Andrade Prates
SEVA ENGENHARIA ELETRÔNICA