I want my project to appear old-school analog but I don’t care what circuits are inside to get the job done. One thing I’ve noticed on my old home stereo is when I use the tuner, a dot flutters on only when a radio station is detected. For example, if the station is 92.3 then the light is on. If I change the dial to 92.1, it will be nothing or even a distorted signal. What I want is to have an LED light up only when I have moved a knob to a clear station, like 92.3. When it’s unclear or nothing, i want the light off - though fluttering on a weak signal would be cool. I just don’t know which circuit module is right for this or if it’s even possible. I have considered if I could pull off the station ID info from the signal or not. I have seen that in the FM module with the display, but I don’t know if there is a way to tie that into a LED switch.
I have read up on some of the documentation but as this is my first time working with these products, I realize the answer might be rather complex. ![]()