detect target_request debugmsgs enable in firmware

I am successfully using openocd’s dcc feature to send my printf msg in my stm32 firmware to the openocd debugger using the code from libdcc … this works well enough for my purposes to replace ITM_SendChar() from the CMSIS which I have used previously (I cannot see any easy to use support for ITM_SendChar in openocd, and I am using SWD interface on the st-link v2 so I am not sure if its even a option on this interface)

The problem is that the ITM_SendChar() routine used to check if both the ITM and ITM port 0 had been enabled before even trying to send the messages, this way it was possible to just leave this code in when debugging or not … however the libdcc stuff has no check so if you make a printf call it will deadlock waiting to send the char’s … does openocd set a flag in one of the dcc cfg registers etc so you know it is connected (or at least has been connected) as I think it is too dangerous to use if by mistake to build a production bit of code without remembering to not define debug?

Alternatively if it is possible to get the ITM_SendChar() sending characters via SWD on the st-link v2 and have the output displayed in gdb that would be even better? … I believe this is better as it is much faster and is buffered better by the core/debugger so there is very low overhead but correct me if I misunderstand please

Thanks