determine the mass loss of PCB using TGA

Hello

To measure mass loss of PCB on drying in order to determine moisture content in PCB as function of temperature, i wanted to use the method of thermogravimetric anlysis TGA ,

This is the TGA that i will use : http://www.komef.ru/files/labsys_evo.pdf

My question is how to know the gaz that i should use inert or reactive gas ? ( especially that the samples heated are PCB with phenolic resin which is sensitive to moisture )

other question : ThE PCB of test is VT-47 with low CTE and high Tg FR-4 (Glass temperature Tg>170°C), so when heating the PCB in the Thermogravimetric analyser, should the heating temperature exceed 170°C or shouldn’t ?

please help me ! it’s urgent! thank you

Have you tried asking the manufacturers\suppliers of the equipment?

It’s the first thing I would do if it was urgent.