Digi Xtend settings

I have 2 900MHz xtend radios set-up in a small office. One is streaming (currently ASCII) data out of a LPC1768. The other is receiving data and going though a USB to serial adapter into a laptop and being displayed on a Putty terminal. Power is set at 100mW. RF and data rates are 115kB. This setup is flawless if the radios are replaced with a cable.

I’m trying to send about 50 ASCII characters at 10Hz. I get a pretty good stream of data to start, sometimes, but then it seems to slow and then stop.

I’m having trouble making sense of the settings listed in the manual. I believe all data related to packetization and data rates are set to the defaults.

Any recommendations on settings? Stuff people have used in the past for this type of blast, wait, blast, wait setup?

10 messages/sec is too much. More like 2 or 3.

More data per message.

Well so much for latency then.

I need to go ahead and go to a binary protocol I believe.