Hi, after several weeks, i’ve successfully executed the ble_freertos_dats/ble_freertos_datc apps in my artemis_thing_plus boards with WDXC_ENABLED/WDXS_ENABLED options in order to perform data streaming and try to measure the achievable data rates between a central and a peripheral device (with MTU=241). In case i change, i.e. the connection interval, the experimental data rate i obtain seems to be ok. however, in case i define CS50_INCLUDED with both 1M PHY and 2M PHY BLE5 modes, the data rates are almost the same … is that correct? … is there any limitation of artemis_thing_plus board which can explain this behaviour?. I would really appreciate any help or any comment related to other experiments regarding this issue.
Best regards