Don't think I am interrupting yet

Deleted code - replaced with post #3

Code deleted - replaced with post #3.

I printed out the Include File for the MSP430f2012 and all of the example files for Timer A. Found a number of errors in my approaches above (now deleted).

This is the present code:

#include “msp430x20x3.h”

;-------------------------------------------------------------------------------

ORG 0F800h ; Program Reset

;-------------------------------------------------------------------------------

RESET: MOV.W #0280h,SP ; Initialize stackpointer

StopWDT MOV.W #05A80h, 0120h ; Stop Watchdog

MOV.W #40, R15 ; Set delay count

SetupP1 BIS.B #001h,&P1DIR ; P1.0 output

SetTA: MOV.W #02A0h, &TACTL ; Set timer A control reg

BIS.B #CPUOFF+GIE, SR

NOP

;Interrupt Service Routines

Intov: ADD &TAIV, PC ; Add offset to PC

RETI ; Vector 0

RETI ; Vector 2

RETI ; Vector 4

RETI ; Vector 6

RETI ; Vector 8

TAovflw: DECD.W R15 ; Vector 10 Timer A overflow

JNZ IntOut

MOV.W #40, R15 ; Reload delay count value

XOR.B #001h,&P1OUT ; Toggle P1.0

IntOut: RETI

;-------------------------------------------------------------------------------

; Interrupt Vectors

;-------------------------------------------------------------------------------

ORG 0FFFEh

DW RESET

ORG 0FFF0h

DW Intov

END

Before I came to the above code I had an error that prevented the CPU from turning off. When I put a scope probe on pin2 I got a square wave of about 10 microseconds period. It was running in a loop.

When I corrected the error the CPU turned off, but does not subsequently wake up as the result of a TA Ovflw interrupt.

Ta Da! It’s working.

I did not enable the Timer Interrupt bit in the Timer Control Register -

MOV.W #02A2h, 0160h