I have a L3G4200D and I’m confused in the unit of its output. I once had a gyro and the sensitivity in the datasheet was mV/deg/s which I could understand, now I read a mdps/digit which is new to me.
My goal is to turn the output from this dps to deg/s. I have the sample code for it and in Arduino program setup I have:
setupL3G4200D(2000);
now in the datasheet for the sensitivity corresponding to this setup we have 70mdps/digit, which I don’t know how to use over an example output of x axis, say, x=619, to deg/s.
//
// This is a simple program for testing the STMicroelectrics 3-axis gyroscope sold by Parallax.
//
// If you are new to the sensor you'll find all you need here. Just rip out what you don't want to save RAM.
//
// If you are using an Arduino Uno R3 like me, connect the SCL line to pin A5. Connect the SDA line to pin A4.
// I don't know anything about the other boards. I'm new to Arduino.
//
// The sample code at Parallax is incorrect in a couple of places. This code follows the application notes from STM. In
// particular I want to note that I found it is very important to check status register 3 to make sure there is new
// data before trying to request it, or else you will get very noisy data.
//
// You can try modifying NUM_GYRO_SAMPLES and GYRO_SIGMA_MULTIPLE.
// These control the statistical averaging that is used to discard bad values.
// The NUM_GYRO_SAMPLES can be reduced for faster calibration, but accuracy will start to suffer if you go below 50 samples.
// Increase the GYRO_SIGMA_MULTIPLE if you have an application that doesn't need to keep track of small rotations.
// Reduce GYRO_SIGMA_MULTIPLE if small rotations are important and you don't mind more noise in the data.
//
// If you are trying to create a compass from the gyro data then use the heading array I added. I found it pretty useful.
// If you set the sensor on your desk and only rotate it in yaw it works great. Turn it upside down and it's a mess, naturally.
//
// If you are putting the sensor in a robot hoping for dead reckoning it might work, but it may be necessary to recalibrate once
// in awhile with the robot stationary. It depends on how long your robot will be driving around and also how bumpy the
// surface is.
//
// Note that if you do not call updateGyro() often enough then you will miss data. You can check for this by looking at
// the status register's 7th bit. If it's on you've missed some data. It's possible to set up an interrupt to catch it. If you
// miss data then the report from the sensor isn't going to work as well for you.
//
// Use share and enjoy this however you like!
//
// Jim Bourke 2/6/2013 (RCGroups.com)
//
#include <Wire.h>
#define CTRL_REG1 0x20
#define CTRL_REG2 0x21
#define CTRL_REG3 0x22
#define CTRL_REG4 0x23
#define CTRL_REG5 0x24
#define CTRL_REG6 0x25
int gyroI2CAddr=105;
int gyroRaw[3]; // raw sensor data, each axis, pretty useless really but here it is.
double gyroDPS[3]; // gyro degrees per second, each axis
float heading[3]={0.0f}; // heading[x], heading[y], heading [z]
int gyroZeroRate[3]; // Calibration data. Needed because the sensor does center at zero, but rather always reports a small amount of rotation on each axis.
int gyroThreshold[3]; // Raw rate change data less than the statistically derived threshold is discarded.
#define NUM_GYRO_SAMPLES 50 // As recommended in STMicro doc
#define GYRO_SIGMA_MULTIPLE 3 // As recommended
float dpsPerDigit=.00875f; // for conversion to degrees per second
void setup() {
Serial.begin(115200);
Wire.begin();
setupGyro();
calibrateGyro();
}
void loop() {
updateGyroValues();
updateHeadings();
//testCalibration();
printDPS();
Serial.print(" --> ");
printHeadings();
Serial.println();
}
void printDPS()
{
Serial.print("DPS X: ");
Serial.print(gyroDPS[0]);
Serial.print(" Y: ");
Serial.print(gyroDPS[1]);
Serial.print(" Z: ");
Serial.print(gyroDPS[2]);
}
void printHeadings()
{
Serial.print("Heading X: ");
Serial.print(heading[0]);
Serial.print(" Y: ");
Serial.print(heading[1]);
Serial.print(" Z: ");
Serial.print(heading[2]);
}
void updateHeadings()
{
float deltaT=getDeltaTMicros();
for (int j=0;j<3;j++)
heading[j] -= (gyroDPS[j]*deltaT)/1000000.0f;
}
// this simply returns the elapsed time since the last call.
unsigned long getDeltaTMicros()
{
static unsigned long lastTime=0;
unsigned long currentTime=micros();
unsigned long deltaT=currentTime-lastTime;
if (deltaT < 0.0)
deltaT=currentTime+(4294967295-lastTime);
lastTime=currentTime;
return deltaT;
}
// I called this from the loop function to see what the right values were for the calibration constants.
// If you are trying to reduce the amount of time needed for calibration just try not to go so low that consecutive
// calibration calls give you completely unrelated data. Some sensors are probably better than others.
void testCalibration()
{
calibrateGyro();
for (int j=0;j<3;j++)
{
Serial.print(gyroZeroRate[j]);
Serial.print(" ");
Serial.print(gyroThreshold[j]);
Serial.print(" ");
}
Serial.println();
return;
}
// The settings here will suffice unless you want to use the interrupt feature.
void setupGyro()
{
gyroWriteI2C(CTRL_REG1, 0x1F); // Turn on all axes, disable power down
gyroWriteI2C(CTRL_REG3, 0x08); // Enable control ready signal
setGyroSensitivity500();
delay(100);
}
// Call this at start up. It's critical that your device is completely stationary during calibration.
// The sensor needs recalibration after lots of movement, lots of idle time, temperature changes, etc, so try to work that in to your design.
void calibrateGyro()
{
long int gyroSums[3]={0};
long int gyroSigma[3]={0};
for (int i=0;i<NUM_GYRO_SAMPLES;i++)
{
updateGyroValues();
for (int j=0;j<3;j++)
{
gyroSums[j]+=gyroRaw[j];
gyroSigma[j]+=gyroRaw[j]*gyroRaw[j];
}
}
for (int j=0;j<3;j++)
{
int averageRate=gyroSums[j]/NUM_GYRO_SAMPLES;
// Per STM docs, we store the average of the samples for each axis and subtract them when we use the data.
gyroZeroRate[j]=averageRate;
// Per STM docs, we create a threshold for each axis based on the standard deviation of the samples times 3.
gyroThreshold[j]=sqrt((double(gyroSigma[j]) / NUM_GYRO_SAMPLES) - (averageRate * averageRate)) * GYRO_SIGMA_MULTIPLE;
}
}
void updateGyroValues() {
while (!(gyroReadI2C(0x27) & B00001000)){} // Without this line you will get bad data occasionally
//if (gyroReadI2C(0x27) & B01000000)
// Serial.println("Data missed! Consider using an interrupt");
int reg=0x28;
for (int j=0;j<3;j++)
{
gyroRaw[j]=(gyroReadI2C(reg) | (gyroReadI2C(reg+1)<<8));
reg+=2;
}
int deltaGyro[3];
for (int j=0;j<3;j++)
{
deltaGyro[j]=gyroRaw[j]-gyroZeroRate[j]; // Use the calibration data to modify the sensor value.
if (abs(deltaGyro[j]) < gyroThreshold[j])
deltaGyro[j]=0;
gyroDPS[j]= dpsPerDigit * deltaGyro[j]; // Multiply the sensor value by the sensitivity factor to get degrees per second.
}
}
void setGyroSensitivity250(void)
{
dpsPerDigit=.00875f;
gyroWriteI2C(CTRL_REG4, 0x80); // Set scale (250 deg/sec)
}
void setGyroSensitivity500(void)
{
dpsPerDigit=.0175f;
gyroWriteI2C(CTRL_REG4, 0x90); // Set scale (500 deg/sec)
}
void setGyroSensitivity2000(void)
{
dpsPerDigit=.07f;
gyroWriteI2C(CTRL_REG4,0xA0);
}
int gyroReadI2C (byte regAddr) {
Wire.beginTransmission(gyroI2CAddr);
Wire.write(regAddr);
Wire.endTransmission();
Wire.requestFrom(gyroI2CAddr, 1);
while(!Wire.available()) {};
return (Wire.read());
}
int gyroWriteI2C( byte regAddr, byte val){
Wire.beginTransmission(gyroI2CAddr);
Wire.write(regAddr);
Wire.write(val);
Wire.endTransmission();
}
This is rather confusing to me. The datasheet specifies the range to be ±2000deg/sec, that the output is 16 bit two’s compliment, and the sensitivity is 0.070deg/sec/bit. These do not match as 2^15 * 0.070 is not 2000 but rather 2293.76.
Does this mean when the sensor has some “head room” above the stated 2000 deg/sec or that after 28571 ADC counts the sensor stops reporting larger numbers?
We have three numbers that are related by an explicit equation that do not compute properly! What gives to make this work?
I figured the dynamic range was limited to +/-2000 deg/sec. Then for some reason (available amps at low supply voltage) they didn’t scale that to fill the full 16 bits. The same is true at the other sensitivities.
Might you get >2000 deg/sec at 3.6v ??? Got me. :think:
That makes some sense. I am trying to do all the math to convert from DAC counts into micro-steps/sec of a paticular stepper motor. My head was swimming with the various factors and that things did not line up. But I think that they simply do not use full ADC range for the dynamic range stated.