Drive hyperdisplay with Artemis Nano? (p.s. Thing Plus - ESP32 WROOM VERY tricky to solder!)

Hi there - I ordered an Artemis Nano for one project, and a hyperdisplay (LCD-15143) and a Thing Plus-ESP32 WROOM for another one. I’m a decent (not amazing) solderer, but in the process of soldering pins onto the Thing Plus I managed to short across from the pins to the chip, and had a bugger of a time undoing it. The spacing between the pin holes and the and the chip are very tight on that board, so be careful when you’re soldering it!

So in the meantime I’m trying to see if I can get my Artemis Nano to drive the hyperdisplay. Got it hooked up, display seems like it’s powering up, got all the libraries installed, example code seemed to upload fine (modulo a ton of warnings like this one:

#warning “No custom configuration supplied for hyperdisplay, using default”), and when I run it, nothing happening at all. Anyone tried to get this board to talk to the hyperdisplay? TIA!

(and fine, my soldering bad, it happens, I’m not asking for a refund - but I tried to re-order the ThingPlus and of course they are backordered! sob)