EagleCad 16F88 - DB9 - RJ45 - 78l05

I feel like I am about to re-invent the wheel for the nth time - Anyone already have an Eagle CAD schematic/board with these components??

Otherwise I will have to start by creating a new library for the 16F88 that I could not find at the EagleCad site.

(I found a user submitted library with 16F688 which is another part I have been using but no 16F88)

Clint

Did you find them? I am looking for a 16f88 library too.

sorry to dig up an old post.

for the 16F88 (or other similar package pics), just use the 18 pin blank IC package and consult the datasheet as to what to hook where.

for the DB9 and RJ45, I’m pretty sure they’re in the libraries already, keep looking! check under connectors - amp

same goes for the 78XX, the TO92 and TO220 packages are in there. I recently made up a D²PAK version if you need it in surface mount. For the SO8 version, just use the SOIC8 blank ic package.

the con-subd library has the DB9 connectors that I always use. I think there are a bunch of RJ45s in the Amp library.

Check this one out

http://thestardestroyer.googlepages.com … eagle.html