For anyone who’s interested in the Allegro A3967 stepper motor driver chip (upon which the EasyDriver is based), I just got a new bench top power supply, so I had to finally test the EasyDriver to see how fast it could go.
Previously, using a small 12V wall wart, I could get around 20,000 steps/second maximum speed. This is with a small NEMA17 stepper motor that is similar to the one SparkFun sells. I drove the EasyDriver with a frequency generator.
At 12V, the EasyDriver gets hot enough that you can’t keep your finger on it. And it smells hot. But it never reaches it’s thermal cutoff of 150C at the die. Surprisingly, even at 20,000 steps/s, it still feels very torquey.
So tonight, I decided that I have enough EasyDrivers lying around here that I could push the input voltage and if it blew up, well, then I’d know where it blew.
So I ran it at 30V. At 10,000 steps/s, the EasyDriver was pulling about 200mA out of my power supply, even when it was set at maximum current. And, guess what. It gets -really- hot. My temperature gun measured the top of the driver at 135C. And then it started shutting down every couple seconds on it’s own. Due to over-heating, I believe. It would then start back up on it’s own after a short time. So the die was getting to 150C.
So, to keep going with the test, I put a small PC fan pointing at the EasyDriver. Then the device temperature was cool enough that you could keep your finger on it no problem. Fans are awesome. Also, without the fan, the little voltage regulator got up to about 110C at 30V input.
At 30V input, I got it all the way up to 44,000 steps/second. If I grabbed the shaft hard, I could get it to stall, so there wasn’t a huge amount of torque up there at that speed. But that’s what you’d expect.
The interesting thing through both of these tests was that because my motor resistance is pretty high (4 ohms per coil), I had to turn the current limit on the EasyDriver as low as it would go in order to get the motor to run smoothly. Oh, it ran at max current, but it was very rough. Gritty, like sand in your scrambled eggs. At minimum current, the EasyDriver was able to generate all 8 microsteps, and even at 44,000 steps/s, it was so smooth you could not even hear it. Couldn’t feel it. No vibration at all. Just a little tape flag that spun so fast it was a blur.
The other test I did tonight (based upon a user’s e-mail question today) was to see if I could fry an EasyDriver by supplying 5V to the STEP and DIR inputs without supplying any power to the EasyDriver. I tried and tried, but was unable to kill the chip. So that doesn’t seem to be one of it’s failure modes, at least the way I was testing it.
Anyway, I’m confident that if I unplugged the motor from the EasyDriver (this was all done on a breadboard) while it was powered at 30V, it would kill the driver chip. However, at 12V, I have been unable to get this driver chip to pop by unplugging the motor while hot, even with hundreds of attempts.
So, this is all just a little bit of info for anyone who’s considering using the EasyDriver for their application. If you need 20-40K steps/second, be prepared to use >12V input and a fan. ![]()
*Brian
PS Just for kicks, I tried plugging and unplugging the motor to the EasyDriver while running at 3K steps/s at 30V input. It turns out that if you plug and unplug it slowly (maybe in for 500ms out for 500ms) then it is fine - it never pops. But when you plug and unplug it as fast as you can (simulating an intermittent open in the wire to the motor) it pops RIGHT away. And it really popped - huge puff of smoke from inside the driver chip, black liquid oozing out from the top of the chip, and a melted spot on the top where the smoke came out. My whole basement smells horrible now. Why-oh-why did I have to push it?!?