I’m using the same microphone and amplifier circuit that is on the Sparkfun Electret Microphone breakout board: https://www.sparkfun.com/products/9964
I built this circuit using the same parts except the microphone is a different part (CMA-4544PF with datasheet at http://www.cui.com/product/resource/cma-4544pf-w.pdf) and VCC is at 3.3V.
I am getting a constant voltage at the output of the microphone. I set the scope to AC coupling with 5 mv/div and I just see noise. I checked all the connections and VCC/ground. I have built this circuit before and it worked, and I have no idea what could be wrong now. Any ideas about common problems or possible sources of error with a circuit like this?
How sure are you that pin 1 of the mic is connected to R1/C1 ? That pin 2 is connected to ground ?
I hope this isn’t too obvious, but is the microphone polarized? How do you tell which is pin 1?
thankyou:
I hope this isn’t too obvious, but is the microphone polarized?
According to the link to the PDF you posted, it is.
thankyou:
How do you tell which is pin 1?
The mechanical drawing at your link shows some sort of green marking nearer to pin 2 than to pin 1.
Haha wow, THANK YOU SO MUCH!!! There is no color on the datasheet I see, but I just read that the metal casing of an electret microphone is grounded. I just measured the resistance from the case to the pin that was presumably ground, and it’s not connected!!! It’s connected to the other pin! So it’s backwards…amazing…