Hey all,
I am restoring an early serial number 1938 Allis Chalmers model B tractor. The sheet metal is in terrible condition with rust and dead paint. I have been using direct current via a small 12 volt battery charger (<10amps) and employing electrolysis to dissolve the rust and loosen the paint. I cut the top off of a plastic 55 gallon drum and made a tank from that, and all the parts fit. This drum is filled with water and sodium carbonate (Arm and Hammer washing soda) for an electrolyte. The solution has a ratio of 1 tablespoon of the sodium carbonate to 1 gallon of water. The process works quite well but slowly. I understand that raising the amperage from the direct current source would speed this up, but buying a large capacity charger is not an option. Buying replacement parts, such as a carburetor and magneto, is already pushing my budget. My question is this; would providing a pulsed width modulation at a high frequency serve to knock the iron oxide molecules loose from the part to be restored faster, or would another method be better?