Thanks for refining your question a little bit. Based on this, let me attempt to try to give you a little more info…
mprev:
My underlying question: Is a modern cheap digital scope more bang for your buck than a older generation used “name brand” scope? Reliability? Maintainability? etc.
While I can’t really speak to the reliability aspect, I can speak to the “bang for the buck” aspect, which ultimately depends on features. Which leads us back to the question that a feature decision really depends on what type of signals you want to measure with the scope.
If you’re primarily going to measure & analyze analog signals - the voltage signal coming out of a power supply, or the waveforms generated by a transmitter, audio work, etc… - any decent analog scope (old or new) will do a good job at this.
By decent you want to make sure that the scope runs fast enough to capture the signal you’re trying to measure (the Mhz of Ghz of the scope), AND it also needs have enough resolution (the amount of data captured per time period) so you can zoom in on the data. If this is your primary area of interest, then I’ve seen many posts recommending purchasing a used name brand scope from eBay (Tek, HP, ar Agilent are 3 brands that come to mind, but there are others).
You can occasionally catch a good deal on great older analog scopes for around 400-500, a decent new one probably starts around 800-1000 (for a name brand).
mprev:
I had originally written off the Saleae Logic device because I could predict hating a PC based tool, and since it’s not realtime I didn’t see much versatility to it. The whole “capture then analyze” seams very foreign to me I’m sure I’d get used to it. In retrospect I’ll probably pick one up.
This question depicts an interest at analyzing digital data. For example, connecting it to an AVR/PIC microcontroller and watching the clock and data on the I/O, UART or I2C pins. Getting a standalone scope that does this type of function really bumps to cost substantially. Scopes that do both Digital Capture/Analysis and Analog Signals are referred to as Mixed Signal Oscilloscopes (MSO), and get very expensive, very quickly. The cheapest way to do this is via a PC based device (and you wont be missing many features either).
There are some newer inexpensive standalone scopes that target this market (Rygol is one that comes to mind) and they do a decent job. Unfortunately, if you really start using them, there’s usually 1 or 2 limitations that will annoy the heck out of you.
You mention ‘realtime’ analysis, and SOME of these PC based devices DO allow you to watch the data in ‘realtime’ (not the Saleae device, but there are other which do allow more “live data”). If you simply want to watch an I/O line toggle between 1 and 0, you can do that on an o-scope AND a some PC-based devices. However, you will find, that whenever you want to analyze complex data, you will need to ‘capture it’ because it’s not humanly possible to view/interpret it quickly enough (digital data can happen way to fast to see). Entire sentences are transmitted in seconds; and no matter how smart you are, you wont be able to count the ones and zeros that quick 
Analyzing data on the “logic” device is just like analyzing the data on my standalone o-scope. Its usually done after the data was already transmitted. If you haven’t seen them, I would highly recommend you check out the videos on Saleae’s website: http://www.saleae.com/logic/videos/.
So in summary - for analog focused - consider a (good condition) used scope on eBay, and for digital data analysis look at PC based devices. Unfortunately, I am not aware of a good ‘entry level-device’ that does both well enough (unless you want to spend 1500+, and even then you’ll be missing features).
Sorry that I rambled on for so long, hopefully this was helpful.