Hi,
i tried to apply the patch for SD/MMC…but when run the command
make ARCH=arm CROSS_COMPILE=arm-linux- uImage
i have this output
make: arm-linux-gcc: Command not found
CHK include/linux/version.h
make[1]: `include/asm-arm/mach-types.h’ is up to date.
CHK include/linux/utsrelease.h
CC arch/arm/kernel/asm-offsets.s
/bin/sh: arm-linux-gcc: command not found
make[1]: *** [arch/arm/kernel/asm-offsets.s] Error 127
make: *** [prepare0] Error 2
I think need the toolchain arm-linux-gcc, but where i find it and how to install?
Thanks
Best regards
You need an build or download an arm toolchain. There are a lot of pre-built toolchains, http://www.schnozzle.org/~coldwell/toolchain/.
I have installed a toolchain and now start the compiler…but show a message:
OBJCOPY arch/arm/boot/zImage
Kernel: arch/arm/boot/zImage is ready
UIMAGE arch/arm/boot/uImage
“mkimage” command not found - U-Boot images will not be built
Image arch/arm/boot/uImage is ready
why the cmd “mkimage” is not found?
Thanks
Best regards
bolatd
4
Hi andreascarlato,
The toolchain you have used is not capable to conver uImage from zImage, due to does not have “mkimage” tool.
You should ELDK (Embedded Linux Development Kit) to build linux kernel without any problem.
You can obtain ELDK from http://www.denx.de/wiki/DULG/ELDKDownloadARM
Sincerely
Bolat DINC