Error After uploading a code with BLE library to artemis ATP board

Hello all,

I have a red board Artimes ATP. I have a BLE application

I uploaded an arduino code to it and gets uploaded fine but when I open the serial monitor, I get the following error

++ MbedOS Fault Handler ++

FaultType: HardFault

Context:

R0: 0

R1: 0

R2: 4

R3: 14ACD

R4: 10001128

R5: 10001158

R6: FFFFFFFF

R7: 0

R8: 0

R9: 0

R10: 0

R11: 0

R12: 0

SP : 10007190

LR : 14AD7

PC : 111FC

xPSR : 1000000

PSP : 10007170

MSP : 1005FF70

CPUID: 410FC241

HFSR : 40000000

MMFSR: 0

BFSR : 82

UFSR : 0

DFSR : 0

AFSR : 0

BFAR : 1C

Mode : Thread

Priv : Privileged

Stack: PSP

– MbedOS Fault Handler –

++ MbedOS Error Info ++

Error Status: 0x80FF013D Code: 317 Module: 255

Error Message: Fault exception

Location: 0x111FC

Error Value: 0x10006180

Current Thread: main Id: 0x10004720 Entry: 0x29505 StackSize: 0x1000 StackMem: 0x100061E0 SP: 0x10007190

For more info, visit: https://mbed.com/s/error?error=0x80FF01 … TEMIS_NANO

– MbedOS Error Info –

Please help!

The link for that error says that means “Error Message: Thread: 0x20001F0C, System is out of memory” - your sketch may be too large?