Error in Sparkfun eagle library? RGB 3mm led

Hi,

I’m wondering if the “rgb 3mm led” of the sparkfun eagle library has an error. This is how the part looks:

http://i.imgur.com/fq7PZ2g.png

The pads are connect. They shouldn’t be, right?

Looks okay in mine. Maybe you need to update your library?

Yea it’s ok here too. Maybe a resolution problem.

I am having the same problem, but with the 5mm LED. The pads are clearly overlapping. Is there a solution to this problem?

https://i.imgur.com/Vq1QYvb.png

Can you edit the pad information?

I have sen this in ther PCB packages, where a pad of a certain size is used in creating the component, whatever the pad is called the software gives it a number (lets say no 80 for this) and then when it is imported into the actual PCB the definitions in the PCB give that pad number (80) a different size.

Perhaps if some of those that have this component looking OK could give the dimensions of the pads they are seeing then you can change them in your pcb to match.