Hi guys, I have an ARM-JTAG and an LPC-P2106-B connected to a laptop running Gentoo 64bit kernel 2.6.22.1, using an ExpressCard/34 parallel port adapter. The parallel adapter shows up as /dev/parport0, and I can use it successfully with some completely different program to bit bang a different board I have. This is what I get when I try to run openocd:
And here is my config file:Info: openocd.c:92 main(): Open On-Chip Debugger (2007-08-10 22:30 CEST)
Error: jtag.c:1253 jtag_examine_chain(): JTAG communication failure, check connection, JTAG interface, target power etc.
Error: jtag.c:1440 jtag_init(): trying to validate configured JTAG chain anyway…
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1346 jtag_validate_chain(): Error validating JTAG scan chain, IR mismatch, scan returned 0x3f
Error: jtag.c:1448 jtag_init(): Could not validate JTAG chain, exit
I am not sure that this config file is completely correct, but I think it should work to at least get farther than this. Any ideas?#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface parport
parport_port 0
parport_cable wiggler
jtag_speed 2
#use combined on interfaces or targets that can’t set TRST/SRST separately
reset_config trst_and_srst srst_pulls_trst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset
#target
#target arm7tdmi
target arm7tdmi little run_and_halt 0 arm7tdmi-s_r4
target_script 0 reset h2294_init.script
run_and_halt_time 0 30
working_area 0 0x40000000 0x40000 nobackup
#flash configuration
flash bank lpc2000 0x0 0x40000 0 0 0 lpc2000_v1 14765 calc_checksum
flash bank cfi 0x80000000 0x400000 2 2 0