ESP32 Micromod + BNO086 IMU = how to connect INT and RST

Good to hear it works !

It does only work when RST is connected to TX0.

That is Correct. RST on the mainboard is a different circuit that you should not use.

No need to do pinMode(). that is already handled by the BN00086 library.


One more question: what does it imply that TX1 and RX1 are now used for the IMU?

I assume that means I cannot add any other hardware that would rely on serial connection, right?

But I can add other Qwiic devices? (Thats what I will do next, display, vibration, audio, led..)

correct. You can add Qwiic / I2C devices.

For everyone else coming here, the solution thanks to @paulvha is:

  1. connect IMU INT to Micromod Mainboard RX1 (lower left next to Micromod slot)
  2. connect IMU RST to Micromod Mainboard TX1 (lower left next to Micromod slot)
  3. on Mainboard, bridge SEC and GND (the 2 pinout holes above RX1 and TX1). I did that with a simple Jumper and a 2-pin pin header)
  4. in sketch define section add:
#define BNO08X_INT RX1
#define BNO08X_RST TX1
  1. in sketch setup section use:
    while (myIMU.begin(BNO08X_ADDR, Wire, BNO08X_INT, BNO08X_RST) == false)

Note that this only works with the single micromod board, the dual board does not have RX1 and TX1.

Without using INT/RST there will be wrong readings, identifyable by checking:
myIMU.getQuatRadianAccuracy();
which in that case is 0.

Do not use the RST pinout from the mainboard itself as mentioned by paulvha.

The Teensy library does not follow the rules of all the other boards. I have not spend enough time to unravel the code to easy understand it. It looks to me that RX should be defined as 0 (or CORE_RXD0_PIN) and TX as 1(or CORE_TXD0_PIN) , but I have not tested it. I am on short leave the coming weeks so do not have the time to invest.