esp8266 connection problem

Hi, i am using ratchet as my websocket server which is based on php and now i am trying to connect it with my esp8266 i tried everything i cant make it work i checked the working of ratchet separately that is with the browser it works perfectly but it always says disconnected in esp8266

can u pls tell me wt is wrong with my code or is the ratchet has to be configured differently for esp8266 ??

arduino code :

#include <Arduino.h>

#include <ESP8266WiFi.h>

#include <WebSocketsClient.h>

#include <Hash.h>

WebSocketsClient webSocket;

#define USE_SERIAL Serial

void webSocketEvent(WStype_t type, uint8_t * payload, size_t length) {

switch(type) {

case WStype_DISCONNECTED:

USE_SERIAL.printf(“[WSc] Disconnected!\n”);

break;

case WStype_CONNECTED: {

USE_SERIAL.printf(“[WSc] Connected to url: %s\n”, payload);

// send message to server when Connected

webSocket.sendTXT(“Connected”);

}

break;

case WStype_TEXT:

USE_SERIAL.printf(“[WSc] get text: %s\n”, payload);

// send message to server

//webSocket.sendTXT(“message here”);

break;

case WStype_BIN:

USE_SERIAL.printf(“[WSc] get binary length: %u\n”, length);

hexdump(payload, length);

// send data to server

// webSocket.sendBIN(payload, length);

break;

}

}

void setup() {

// USE_SERIAL.begin(921600);

USE_SERIAL.begin(115200);

//Serial.setDebugOutput(true);

USE_SERIAL.setDebugOutput(true);

USE_SERIAL.println();

USE_SERIAL.println();

USE_SERIAL.println();

for(uint8_t t = 4; t > 0; t–) {

USE_SERIAL.printf(“[SETUP] BOOT WAIT %d…\n”, t);

USE_SERIAL.flush();

delay(1000);

}

const char* ssid = “…”;

const char* password = “…”;

WiFi.begin(ssid, password);

while (WiFi.status() != WL_CONNECTED) {

delay(500);

Serial.print(“.”);

}

// server address, port and URL

webSocket.begin(“192.x.x.x”, 9000, “/”);

// event handler

webSocket.onEvent(webSocketEvent);

// try ever 5000 again if connection has failed

webSocket.setReconnectInterval(5000);

}

void loop() {

webSocket.loop();

}