ESP8266 Return LED Signal?

Hello All,

Working on a Poofer project, or something similar (see: ESP8266 Powered Propane Poofer - SparkFun Learn). I want to wirelessly activate a propane fire pit, and have a flame-out indicator send a signal back to the app if no flame is detected.

TL;DR: Trying to get a “return signal” from my “FLAME OUT” LED back through the DEV board to show in the App.

Instead of manually operating the Igniter and Solenoid(s), I have a flame controller that I will be switching On/Off with the Dev Board via a relay. The controller is able to automatically switch on the Igniter and Solenoids, and includes a flame sensor that monitors if there is flame present. If there is not flame present (flame blows out, out of fuel, etc) the controller will (temporarily) shut down the solenoid/fuel flow for safety, and activate an LED light/send a signal through a 1/4" tab that tells the operator there is no flame.

HOW DO I GET THIS (RETURN) SIGNAL BACK THROUGH THE DEV BOARD TO SHOW IN MY APP??

Either the flame controller signal-out wire can attach directly to the DEV Board, or I can have that signal out wire connect to a relay, and then attach to the DEV Board. Question is: is this possible/is it possible to send a signal TO the Dev Board and then have it show up as active/ON in the app? And then turn OFF when the signal is lost (indicating flame is again present)??

Thanks for your help!

@Nick_SparkX would really appreciate your help because you’re the GOAT with this stuff!

Hey! I’m happy to have a look!
Are you using the ESP8266 and the ESP8266WiFi Library like in my project or are you on another platform?

If you’re using something similar to the example code, you’ll notice that the app is really just a webpage that you’re building out of Strings and then serving over the WiFi, so all you need to do is connect the flame out LED to an input pin (either directly or using a relay or a transistor) and then digitalRead() that pin while you’re building the webpage.

In the example code for the propane poofer, you’ll see a line like this:

if ( digitalRead(IGNITION_PIN) == 0 ){
  s += "Ignitior is currently turned OFF.";}
  else{
  s += "Ignitior is currently turned ON.";}
  s += "<br><br>\r\n"; // Go to the next line.

You could use the same structure, for example, and do this:

if ( digitalRead(FLAMEOUT_PIN) == 1 ){
  s += "Flame Out Detected";}
  s += "<br><br>\r\n"; // Go to the next line.

This just adds a line of text to the page that says “Flame Out Detected” whenever that pin goes high. Of course you could put whatever HTML there that you wanted, so it could show an alert box or a selected radio button or an emoji or whatever looks better than a line of text.

Thank you @Nick_SparkX and @emberjune !! I will update as the project progresses